您好!
从手册可以看到,在–40°C ≤ TJ ≤ +85°C下Vout=1V@750mA压差有1150mV,实际真的有这么大吗?我在Ta=25℃下测试时,测量到还是1V,并没有压差,是到高温下才会出现吗?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,通过查阅资料发现您上面给的效率公式不对,查阅资料的效率计算公式如下:

所以按照查阅到的资料计算效率=(1V*0.75A)/(5V*0.2A)*100%=75% 注:5V输入的电流为0.2A是我预估的
按照我上面计算出来的效率为75%,才是一个正常的效率,也可以解释Figure 5-13. Load Regulation vs IOUT表格,在是可以实现输出Vout=1V/Iout=750mA,只是实际Vout的值为0.96V。按照您给出的公式效率为0.18是不正常的数值。
请问我以上的理解正确吗?