This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV757P: 输入5V输出1V@750mA压差有多大?

Part Number: TLV757P

您好!

从手册可以看到,在–40°C ≤ TJ ≤ +85°C下Vout=1V@750mA压差有1150mV,实际真的有这么大吗?我在Ta=25℃下测试时,测量到还是1V,并没有压差,是到高温下才会出现吗?