各位专家:
本人在使用LM5119时遇到一个比较棘手的问题。在使用二极管仿真模式()时,空载时LO仍然会发一个脉宽约200ns的PWM波,且在输出负载为半载时,此PWM波仍然为200ns左右。请问此种情况是如何产生,又该如何解决呢?
原理参数如图所示交错buck.pdf
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位专家:
本人在使用LM5119时遇到一个比较棘手的问题。在使用二极管仿真模式()时,空载时LO仍然会发一个脉宽约200ns的PWM波,且在输出负载为半载时,此PWM波仍然为200ns左右。请问此种情况是如何产生,又该如何解决呢?
原理参数如图所示交错buck.pdf
项目背景如下:
输入36V,输出28V/500W,采用LM5119交错buck方案。
启用二极管仿真模式(DEMB接地)后不同负载下两个LO的波形如下:

上图为36V输入,空载时两个LO的波形

上图为36V输入,输出28V/3A时的两个LO的波形

上图为输入36V,输出28V/9A时两个LO的波形
存在问题:
1、空载时为何LO会出脉冲?
2、重载时LO的占空比应为19%左右,为何无论空载重载LO的占空比不变?
3、因为启用二极管仿真模式一直有问题,所以转为完全的同步整流模式,但是在高压输入时空载损耗太大不能接受, 有什么措施能减少输入空载损耗?
请TI的专家帮忙看一下,感谢!