This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5119: 二极管仿真模式的问题

Part Number: LM5119


各位专家:

     本人在使用LM5119时遇到一个比较棘手的问题。在使用二极管仿真模式()时,空载时LO仍然会发一个脉宽约200ns的PWM波,且在输出负载为半载时,此PWM波仍然为200ns左右。请问此种情况是如何产生,又该如何解决呢?

原理参数如图所示交错buck.pdf

  • 项目背景如下:

    输入36V,输出28V/500W,采用LM5119交错buck方案。

    启用二极管仿真模式(DEMB接地)后不同负载下两个LO的波形如下:

    上图为36V输入,空载时两个LO的波形

    上图为36V输入,输出28V/3A时的两个LO的波形

    上图为输入36V,输出28V/9A时两个LO的波形

    存在问题:

    1、空载时为何LO会出脉冲?

    2、重载时LO的占空比应为19%左右,为何无论空载重载LO的占空比不变?

    3、因为启用二极管仿真模式一直有问题,所以转为完全的同步整流模式,但是在高压输入时空载损耗太大不能接受, 有什么措施能减少输入空载损耗?

    请TI的专家帮忙看一下,感谢!