谢谢
2012-4-11
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢
2012-4-11
TMIN用来设置最小占空比。具体设置方法是在该引脚与GND之间下拉一颗电阻。公式请参考datasheet的18页。
RSUM用来选择反馈模式是电压模式还是电流模式。如果是电压模式,需要上拉到Vref,上拉电阻的值决定了cycle-by-cycle保护的值;如果是电流模式,需要下拉到GND,此时该电阻出了cycle-by-cycle,还用作斜坡补偿。而相关的公式在datasheet中有详尽描述。
DCM用来设置同步整流与非同步整流的切换的值,包括回滞。公式参考datasheet的22页。
DELAB DELCD和ADEL用来设置死区时间,在datasheet的14页有详细描述。
电压模式下,CS关断输出的电压时2V;但在电流模式下,CS引脚会叠加一个补偿电压,此时,有可能CS还未达到2V,输出就已经关断。因为内部关断输出的阈值是2V。datasheet的22页有详细的框图。
电压模式时,斜坡添加到了cycle-by-cycle,因此,要考虑负载来决定斜坡的值,防止驱动被提前关断。