This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25756: 反向运行及并联运行的问题

Part Number: BQ25756

BQ25756工作在在反向的放电模式下,此时Vbat为系统的输入电压源,Vvac为系统的输出母线电压,反向放电的终止条件是什么,什么时候终止放电,是Vbat下降到3V以下吗?手册中有一句:“When VVAC falls below the undervoltage threshold (programmable via SYSREV_UV register bit), the device stops switching, clears the EN_REV bit, and exits Reverse mode. ”但是这是欠压保护以终止反向模式,而且是VVAC与SYSREV_UV比较然后触发系统反向模式下的欠压保护,系统跳出反向模式。在正常的反向放电模式下,VVAC如果一直在系统正常运行范围内,如何终止放电。 

此外,两个BQ25756并联,需不需要采取均流措施?

  • 您好

    关于你提到的BQ25756在反向放电模式下的终止条件,根据技术手册和相关资料,当VVAC下降到欠压阈值(这个阈值可以通过SYSREV_UV寄存器位进行编程设置)以下时,设备会停止切换,清除EN_REV位,并退出反向模式。所以,并不是Vbat下降到3V以下才终止放电,而是VVAC与设置的欠压阈值进行比较,当VVAC低于该阈值时触发系统反向模式下的欠压保护,从而跳出反向模式。

    至于两个BQ25756并联时是否需要采取均流措施,答案是肯定的。在并联电路中,为了保证每个单元分担的电流相对均匀,避免某个单元过载或轻载,通常需要采取均流措施。对于BQ25756这样的开关电源控制器,可以采取多种均流方法,比如使用独立的PWM控制器,通过电流采样反馈到PWM控制器的相关引脚来调节输出电压,从而达到均流的目的。此外,还可以使用简单的RC网络检测电流大小,并通过平均值均流法或最大值均流法等方法来实现均流。

  • 那在反向CV放电时,VVAC电压是恒定的啊,怎么终止?

  • 您好

    在反向CV(恒压)放电模式下,BQ25756通过调节输入端子电压或监测电池电压和电流来实现放电的终止。技术手册中提到,该设备在反向模式下会从电池中获取电力,并通过添加的恒定电流环路来调节输入端子电压,从而实现保护。这意味着,即使VVAC电压恒定,当达到某些条件时,放电过程也会终止。

    具体来说,BQ25756具有一些相关的寄存器设置,如REG0x0A_Reverse_Mode_Input_Current_Limit和REG0x0C_Reverse_Mode_Input_Voltage_Limit,这些寄存器用于设置反向模式下的输入电流和电压限制。当实际放电过程中的电流或电压超过这些设置的限制时,设备可能会采取保护措施,如降低放电电流或终止放电。

    此外,技术手册还提到了其他与充电和放电终止相关的寄存器设置,如REG0x14_Precharge_and_Termination_Control,该寄存器允许用户设定预充电流的大小以及何时停止充电流程。虽然这主要针对充电过程,但类似的原则也可能适用于反向放电模式下的终止条件设置。

  • OK,谢谢。另外, 我再想问下,反向模式下的电池放电电流能控制恒定么,手册上说反向模式下的IAC_REV和VAC_REV是可调节的,能够运行于CC/CV,“The charger also monitors and regulates the battery discharging current in reverse mode. When the battery
    discharge current rises above the IBAT_REV register setting, the charger reduces the reverse mode power flow
    to limit the discharge current.”,当电池电流超过IBAT_REV寄存器设定值时,将降低放电电流,但是能保持Ibat恒定么

  • 您好

    根据datasheet上的说明 应该不会保持,但是不会超过配置的相关范围。如果您想做成恒定要进行相关寄存器的配置以及电路的限制。

  • 需要配置哪些寄存器和电路啊

  • 您好

    请参考这个寄存器以及考察包括电池的内阻、外部负载的阻抗以及BQ25756自身的调节能力。做出针对性的匹配和配置。

  • 嗯嗯,谢谢,我准备把Rbat_sns出口的SRP和SRN同时连接到ACN和ACP,这样反向模式下,IAC_REG的控制的电流实际就是Battery的放电电流了,控制其为恒定。