This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS3762: TPS3762D02OVDDFR 中D的含义

Part Number: TPS3762


您好,

我们计划使用TPS3762做60V电源过压检测,现需要确认一下型号命名中“D” 的含义。

“UV Bypass”是指不具有欠压检测功能;

“BIST RESET Trigger”是指在BIST内部诊断时,RESET_BAR和BIST_BAR会被同时拉低。(功能时序图参考图7-8而不是7-9)

请教以上理解是正确的吗?谢谢。