Part Number: J722SXH01EVM
Is the DSPLIB_cascadeBiquad equal to DSPF_sp_biquad ,
How should I set the params?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: J722SXH01EVM
Is the DSPLIB_cascadeBiquad equal to DSPF_sp_biquad ,
How should I set the params?
Hi,
Could you please refer this : https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1619770/faq-tda4vh-q1-dsplib-mathlib-steps-to-migrate-c66x-source-code-to-c7x
I will go through the remaining questions from my end and respond to you shortly.
As mentioned earlier, we cannot directly use the cascade biquad code from DSPLIB for sp_biquad. It will behave the same as sp_biquad only if the required modifications are applied.
1) numStages = 1, DSPF_sp_biquad processes one biquad stage per call.
2) Coeff layout :
DSPF_sp_biquad -->
b = {b0,b1,b2}
a = {1,a1,a2}
DSPLIB_cascadeBiquad_exec --->
coeff = {b0,b1,b2,a2,a1}
3) Align Filter state representation :
DSPF_sp_biquad -->
delay [0] , delay[1]
DSPLIB_cascadeBiquad_exec --->
vd0, vd1 per stage.
4) Simplify the multistage pipeline ->
Kept only stage1 logic and removed remaining stages.
5) Remove output gain scaling as we only use single stage.
ie, output = y
6) Input/Output Buffer Access -
numChannels = 1
dataBufferInPitch = 1
dataBufferOutPitch = 1
Please refer to the test code attached below for these changes.
void DSPF_sp_biquad(float *x, float *b, float *a,
float *delay, float *y, const int nx)
{
int i;
for (i = 0; i < nx; i++)
{
y[i] = b[0] * x[i] + delay[0];
delay[0] = b[1] * x[i] - a[1] * y[i] + delay[1];
delay[1] = b[2] * x[i] - a[2] * y[i];
}
}
/* ====================================================================================================
C7x Cascade Biquad
======================================================================================================= */
typedef void* DSPLIB_kernelHandle;
typedef struct {
uint32_t dataSize;
uint32_t numStages;
uint32_t numChannels;
} DSPLIB_cascadeBiquad_InitArgs;
typedef struct {
DSPLIB_cascadeBiquad_InitArgs initArgs;
uint32_t dataBufferInPitch;
uint32_t dataBufferOutPitch;
uint32_t filterVarPitch;
} DSPLIB_cascadeBiquad_PrivArgs;
template <typename dataType>
void DSPLIB_cascadeBiquad_exec(
DSPLIB_kernelHandle handle,
void *pIn,
void *pFilterCoeff,
void *pFilterVar,
void *pOut)
{
DSPLIB_cascadeBiquad_PrivArgs *args =
(DSPLIB_cascadeBiquad_PrivArgs*)handle;
dataType *input = (dataType*)pIn;
dataType *coeff = (dataType*)pFilterCoeff;
dataType *state = (dataType*)pFilterVar;
dataType *output = (dataType*)pOut;
int N = args->initArgs.dataSize;
dataType b0 = coeff[0];
dataType b1 = coeff[1];
dataType b2 = coeff[2];
dataType a1 = coeff[3];
dataType a2 = coeff[4];
dataType d0 = state[0];
dataType d1 = state[1];
for(int i=0;i<N;i++)
{
dataType x = input[i];
dataType y = b0*x + d0;
d0 = b1*x - a1*y + d1;
d1 = b2*x - a2*y;
output[i] = y;
}
state[0] = d0;
state[1] = d1;
}
If you intend to port the C66x sp_biquad implementation to C7x, you can follow the steps provided in the FAQ [ https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1619770/faq-tda4vh-q1-dsplib-mathlib-steps-to-migrate-c66x-source-code-to-c7x]. The FAQ also includes training material that explains how to configure the streaming engine parameters.