This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

J722SXH01EVM: Is there a function in c7000 dsplib equal to DSPF_sp_biquad in C6000 dsplib

Part Number: J722SXH01EVM

Is the DSPLIB_cascadeBiquad equal to DSPF_sp_biquad ,

How should I set the params?

 

  • Hi,

    We have received your post and the investigation will take some time. Thank you for your patience.

  • Hi,

    Could you please refer this : https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1619770/faq-tda4vh-q1-dsplib-mathlib-steps-to-migrate-c66x-source-code-to-c7x 

    I will go through the remaining questions from my end and respond to you shortly.

  • I did not find someting to do with the  dsplib biquadfunction

  • I did not find someting to do with the biquad function in dsplib

  • As mentioned earlier, we cannot directly use the cascade biquad code from DSPLIB for sp_biquad. It will behave the same as sp_biquad only if the required modifications are applied.

    1) numStages = 1, DSPF_sp_biquad processes one biquad stage per call.
    
    2) Coeff layout :
       DSPF_sp_biquad --> 
       b = {b0,b1,b2}
       a = {1,a1,a2}
       DSPLIB_cascadeBiquad_exec --->
       coeff = {b0,b1,b2,a2,a1}
    3) Align Filter state representation :
       DSPF_sp_biquad -->
       delay [0] , delay[1]
       DSPLIB_cascadeBiquad_exec --->
       vd0, vd1 per stage.
    4) Simplify the multistage pipeline ->
       Kept only stage1 logic and removed remaining stages.
    5) Remove output gain scaling as we only use single stage.
       ie, output = y
    6) Input/Output Buffer Access -
       numChannels = 1
       dataBufferInPitch = 1
       dataBufferOutPitch = 1

    Please refer to the test code attached below for these changes.

    void DSPF_sp_biquad(float *x, float *b, float *a,
        float *delay, float *y, const int nx)
    {
        int i;
    
        for (i = 0; i < nx; i++)
        {
            y[i] = b[0] * x[i] + delay[0];
            delay[0] = b[1] * x[i] - a[1] * y[i] + delay[1];
            delay[1] = b[2] * x[i] - a[2] * y[i]; 
        }
    }
    
    /* ====================================================================================================
                                             C7x Cascade Biquad
    ======================================================================================================= */
    typedef void* DSPLIB_kernelHandle;
    
    typedef struct {
        uint32_t dataSize;
        uint32_t numStages;
        uint32_t numChannels;
    } DSPLIB_cascadeBiquad_InitArgs;
    
    typedef struct {
        DSPLIB_cascadeBiquad_InitArgs initArgs;
        uint32_t dataBufferInPitch;
        uint32_t dataBufferOutPitch;
        uint32_t filterVarPitch;
    } DSPLIB_cascadeBiquad_PrivArgs;
    
    template <typename dataType>
    void DSPLIB_cascadeBiquad_exec(
            DSPLIB_kernelHandle handle,
            void *pIn,
            void *pFilterCoeff,
            void *pFilterVar,
            void *pOut)
    {
        DSPLIB_cascadeBiquad_PrivArgs *args =
            (DSPLIB_cascadeBiquad_PrivArgs*)handle;
    
        dataType *input = (dataType*)pIn;
        dataType *coeff = (dataType*)pFilterCoeff;
        dataType *state = (dataType*)pFilterVar;
        dataType *output = (dataType*)pOut;
    
        int N = args->initArgs.dataSize;
    
        dataType b0 = coeff[0];
        dataType b1 = coeff[1];
        dataType b2 = coeff[2];
        dataType a1 = coeff[3];
        dataType a2 = coeff[4];
    
        dataType d0 = state[0];
        dataType d1 = state[1];
    
        for(int i=0;i<N;i++)
        {
            dataType x = input[i];
    
            dataType y = b0*x + d0;
    
            d0 = b1*x - a1*y + d1;
            d1 = b2*x - a2*y;
    
            output[i] = y;
        }
    
        state[0] = d0;
        state[1] = d1;
    }

    If you intend to port the C66x sp_biquad implementation to C7x, you can follow the steps provided in the FAQ [ https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1619770/faq-tda4vh-q1-dsplib-mathlib-steps-to-migrate-c66x-source-code-to-c7x]. The FAQ also includes training material that explains how to configure the streaming engine parameters.