This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请教C6657电源配置问题

Other Parts Discussed in Thread: LM10011, TPS54525

问题描述:

系统选用C6657作为主处理器,C6657电源及外设参照其开发板设计,每一路电源由电源芯片TPS54525PWP产生,由一片CPLD控制上电顺序,见原理图。其中CVDD电压由TPS54525+LM10011产生,并且通过C6657 SmartReflex功能控制。

现在的问题是,系统所有电源上电完成后,通过JTAG访问C6657内部寄存器或者通过gel文件加载配置,部分电路板出现部分寄存器(主要是DDR相关寄存器)访问异常的情况。通过调整LM10011芯片SET管脚的配置电路调整CVDD电压,出现上述问题的部分电路板可以正常工作,但是仍有一部分电路板问题得不到改善。

所以请教以下问题:

1、 出现上述问题可能是什么原因造成的?

2、 关于CVDD电压生成电路是否有问题?

3、 关于SmartReflex通过LM10011调节CVDD电压的问题描述请见附件二,为什么会出现这种情况?

附件二:图像系统电路板调试smartflex问题.docx
  • LM10011在C6657启动之前应输出1.1V电压, 0.811V电压太低,DSP很大可能不能正常工作,是否电源供电不够,CVDD要求的电流比较大,请使用 http://www.ti.com/lit/zip/sprm600 工具计算电流值,保证供电电流足够。