This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

C6657 RBL boot with DDR3

您好,Ti的攻城狮:

      有个问题想咨询一下,我们已经使用C6657有一段时间了,单核双核,SPI RBL加载使用都正常。现在我们编写的程序可能有点大,其中text段程序是放在SL2段中,0核1核分别跑不同程序,怕以后SL2段不够用,想在想在SPI boot的基础上把DDR3加进去,然后就不成功。

      问题1:在论坛看到有些资料说C6657 RBL方式支持DDR3 Level,但是有些不支持,就比较糊,想请工程师给个正儿八经的链接。

      问题2:SPI BOOT with DDR3使用的转换工具里面有个工具叫AddDDRTable,其中有120个Bit是DDR3初始化寄存器的值。这个工具是可以用的么?有没有文档对着120个Bit具体含义进行说明?

      问题3:之前又在论坛看到个文档,主程序定义了一段#program ddr_emif的程序段,里面是DDR3寄存器初始化的值,然后映射到cmd里面的DDR_Config,不是很懂这个的意思?

  • 1、For C6657 device, the DDR PLL initialization sequence was chnaged after the bootROM code was finalized and also BootROM doesn`t support many features like DDR hardware leveling, etc so our recommendation for user who want to load code in DDR is to setup a lower DDR clock using boot ROM and boot the device and then increase the DDR clock when the application boots up.
    e2e.ti.com/.../493269
    2、查一下6657 SDK tiboot_c665x.h文件,里面bootEmif4Tbl_s有对DDR configuration table的解释.
    3、哪个文档?
  • 1. tiboot_c665x.h头文件中对DDR的描述
    typedef struct bootEmif4Tbl_s {
    UINT32 configSelect_msw; /* Bit map defining which registers to set */
    UINT32 configSelect_slsw; /* Bit map defining which registers to set */
    UINT32 configSelect_lsw; /* Bit map defining which registers to set */

    UINT32 pllPrediv; /* Values of all 0s will disable the pll */
    UINT32 pllMult;
    UINT32 pllPostDiv;

    UINT32 sdRamConfig; /* Controlled by bit 1 of configSelect_msw */
    UINT32 sdRamConfig2; /* Bit 2 */
    UINT32 sdRamRefreshCtl; /* Bit 3 */
    UINT32 sdRamTiming1; /* Bit 4 */
    UINT32 sdRamTiming2; /* Bit 5 */
    UINT32 sdRamTiming3; /* Bit 6 */
    UINT32 lpDdrNvmTiming; /* Bit 7 */
    UINT32 powerManageCtl; /* Bit 8 */
    UINT32 iODFTTestLogic; /* Bit 9 */
    UINT32 performCountCfg; /* Bit 10 */
    UINT32 performCountMstRegSel; /* Bit 11 */
    UINT32 readIdleCtl; /* Bit 12 */
    UINT32 sysVbusmIntEnSet; /* Bit 13 */
    UINT32 sdRamOutImpdedCalCfg; /* Bit 14 */
    UINT32 tempAlterCfg; /* Bit 15 */
    UINT32 ddrPhyCtl1; /* Bit 16 */
    UINT32 ddrPhyCtl2; /* Bit 17 */
    UINT32 priClassSvceMap; /* Bit 18 */
    UINT32 mstId2ClsSvce1Map; /* Bit 19 */
    UINT32 mstId2ClsSvce2Map; /* Bit 20 */
    UINT32 eccCtl; /* Bit 21 */
    UINT32 eccRange1; /* Bit 22 */
    UINT32 eccRange2; /* Bit 23 */
    UINT32 rdWrtExcThresh; /* Bit 24 */

    UINT32 chipConfig[64];

    } BOOT_EMIF4_TBL_T;

    2. 然后我根据这个结构体猜测了一下AddDDRTable的参数含义,
    第一行0x00000070 不知道是干嘛的
    第二行0x008FFD20 where to load ddr to L2,我没有找到有手册对6657的地址进行说明(6670 6678我找到了)
    时钟速率我配置的是156.25*20/3=1041.6666(标准1066,1333,1600)
    /*
    DDR3 table paramater config
    total 120 words
    The DDR configuration table location defined by Boot ROM:
    C6678: 0x00873500
    C6657: 0x008FFD20
    */

    0x00, 0x00, 0x00, 0x70, // ???不知道干嘛的
    0x00, 0x8F, 0xFD, 0x20, // where to load ddr to L2

    0x02, 0x42, 0x80, 0xF5, // config select: Bitmap definig which registers to set
    0000 0010 0100 0010 0100 0000 1111 0101 //24bit‬‬猜测0有效

    0x00, 0x00, 0x00, 0x00, // pll Prediv--Controlled by bit 1 of configSelect_msw
    0x00, 0x00, 0x00, 0x13, // pll mul 156.25*20/3=1041.6666
    0x00, 0x00, 0x00, 0x02, // pll post div
    0x63, 0x02, 0xAA, 0xB2, //0 sd ram config
    0x00, 0x00, 0x00, 0x00, //0 sd ram config2
    0x00, 0x00, 0x51, 0x56, //0 sdram fresh cntrl
    0x11, 0x13, 0x78, 0x3C, //0 sdram timing 1
    0x30, 0x4F, 0x55, 0x23, //0 sdram timing 2
    0x55, 0x95, 0x06, 0xAF, //0 sdram timing 3
    0x00, 0x00, 0x00, 0x00, //1 lpDdrNvmTiming
    0x00, 0x00, 0x00, 0x00, //0 powerManageCtl
    0x00, 0x00, 0x00, 0x00, //0 iODFTTestLogic
    0x00, 0x01, 0x00, 0x00, //1 oerform count config
    0x00, 0x00, 0x00, 0x00, //0 performCountMstRegSel
    0x00, 0x00, 0x00, 0x00, //0 readIdleCtl
    0x00, 0x00, 0x00, 0x00, //0 sysVbusmIntEnSet
    0x70, 0x07, 0x32, 0x14, //0 sdRamoutImppedCalcfg
    0x00, 0x00, 0x00, 0x00, //1 tempAlterCfg
    0x00, 0x10, 0x01, 0x0F, //0 ddrPhyCtl1
    0x00, 0x00, 0x00, 0x00, //0 ddrPhyCtl2
    0x00, 0x00, 0x00, 0x00, //1 priClassSvceMap
    0x00, 0x00, 0x00, 0x00, //0 mstId2ClsSvce1Map
    0x00, 0x00, 0x00, 0x00, //0 mstId2ClsSvce2Map
    0x10, 0x00, 0x00, 0x00, //0 ecc cntrl
    0x00, 0x00, 0x00, 0x00, //0 eccRange1
    0x00, 0x00, 0x00, 0x00, //0 eccRange2
    0x00, 0x00, 0x03, 0x05 //0 rdWrtExcThresh

    3. 这是我使用的cmd文件,只是将text段挪到DDR3,gel初始化DDR3(no boot),main函数中没有初始DDR3,debug下程序正常运行。固化SPI加载不得行。
    -heap 0x800
    -stack 0x1000

    //cmd
    MEMORY
    {
    /* Local L2, 0.5~1MB*/
    VECTORS: o = 0x10800000 l = 0x00000200
    LL2_RW_DATA: o = 0x10800200 l = 0x000DFF00
    //DDR_CFG: o = 0x108ffd20 l = 0x180

    /* Shared L2 1MB for C6657*/
    SL2: o = 0x0C000000 l = 0x001FFFFF

    /* External DDR3, upto 2GB per core */
    DDR3_CODE: o = 0x80000000 l = 0x01000000 /*set memory protection attribitue as execution only*/
    DDR3_R_DATA: o = 0x81000000 l = 0x01000000 /*set memory protection attribitue as read only*/
    DDR3_RW_DATA: o = 0x82000000 l = 0x06000000 /*set memory protection attribitue as read/write*/
    EMIF16_DATA:o = 0x70000000 l = 0x10000000 /* EMIF16 memory space */
    }

    SECTIONS
    {
    vecs > VECTORS

    //.emif4Cfg > DDR_CFG
    .text> DDR3_RW_DATA
    .cinit> SL2
    .const> SL2
    .switch > SL2

    .stack> LL2_RW_DATA
    GROUP
    {
    .neardata
    .rodata
    .bss
    } > LL2_RW_DATA
    .far:testBuf > LL2_RW_DATA
    .far> LL2_RW_DATA
    .fardata > LL2_RW_DATA
    .cio> LL2_RW_DATA
    .sysmem> LL2_RW_DATA

    }