This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在学习DVRRDK,看了一下MCFW的demo基本流程理解,也可以仿照demo修改,但是涉及到底层一点(link)的还是不理解。
现在学习link,发现link牵涉到的内容比较广,相应资料比较少,一些介绍得也很抽象。
能给写学习link的建议吗?如果有详细的资料希望可以共享一下,怎样阅读link相关的代码学习效率比较高。
这个文档看完后了?因为刚开始接触,之前也没有相应的学习经历。我把Docs下的文档基本上都过了,对整体框架还是有了解,知道多核之间的分工,以及相互间的通信机制。但是具体到代码级就乱了,看了mcfw下的demo程序也没有感觉收获多大。我想做的工作是将自己的图像算法移植到DM8168上,但是编程从哪里开始,怎么开始还是一点不清楚。不知道能不能给点具体建议啊。
在哪里能下到新版的sdk啊,我的是dvrrdk3.0的,但是里面的mcfw下的demo运行有问题,[host] MCFW_IPCFRAMES:VcapVenc_ipcFramesSendRecvFxn:Entered... [m3vpss ] 127346: Assertion @ Line: 464 in links_m3vpss/system/system_dctrl.c: retVal == FVID2_SOK : failed !!!应该怎么解决呢?