This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DM8168怎样学习DVRRDK下的MCFW架构和link



最近在学习DVRRDK,看了一下MCFW的demo基本流程理解,也可以仿照demo修改,但是涉及到底层一点(link)的还是不理解。

现在学习link,发现link牵涉到的内容比较广,相应资料比较少,一些介绍得也很抽象。

能给写学习link的建议吗?如果有详细的资料希望可以共享一下,怎样阅读link相关的代码学习效率比较高。

  • 你好!

      在\dvr_rdk\docs\Trainings下面有一个《DVR_RDK_McFW_Link_API_Training》的文档,可以先看看。

  • 这个文档看完后了?因为刚开始接触,之前也没有相应的学习经历。我把Docs下的文档基本上都过了,对整体框架还是有了解,知道多核之间的分工,以及相互间的通信机制。但是具体到代码级就乱了,看了mcfw下的demo程序也没有感觉收获多大。我想做的工作是将自己的图像算法移植到DM8168上,但是编程从哪里开始,怎么开始还是一点不清楚。不知道能不能给点具体建议啊。

  • 在哪里能下到新版的sdk啊,我的是dvrrdk3.0的,但是里面的mcfw下的demo运行有问题,[host] MCFW_IPCFRAMES:VcapVenc_ipcFramesSendRecvFxn:Entered... [m3vpss ]  127346: Assertion @ Line: 464 in links_m3vpss/system/system_dctrl.c: retVal == FVID2_SOK : failed !!!应该怎么解决呢?

  • 您好,我的软件版本是IPNC_RDK3.8。说明文档没有DVR_RDK全,请问您能发给我一下McFW相关的说明文档吗?感激不尽