SPRU733A 416页 ,两个例子要表达什么意思?
这个程序一定是并行执行的吗?
LDW .D1 *A0,A1
ADD .L1 A1,A2,A3 不就是A1先赋值成10,然后和A2相加给A3吗?
怎么datasheet上边的解释说这样就错了呢?
如果两个指令之间产生中断,停止都停止,执行都同时执行,又有什么问题呢?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
SPRU733A 416页 ,两个例子要表达什么意思?
这个程序一定是并行执行的吗?
LDW .D1 *A0,A1
ADD .L1 A1,A2,A3 不就是A1先赋值成10,然后和A2相加给A3吗?
怎么datasheet上边的解释说这样就错了呢?
如果两个指令之间产生中断,停止都停止,执行都同时执行,又有什么问题呢?
你好,并不是如你理解的
“LDW .D1 *A0,A1
ADD .L1 A1,A2,A3 不就是A1先赋值成10,然后和A2相加给A3吗?”
这里的情况是:The ADD instruction, which is in a delay slot of the LDW , sums A2 with the value in A1 (0) and the result in A3 is just a copy of A2.
ADD指令并没有使用LDW指令的结果,即没有使用A1赋值的结果,而是使用A1之前的值。