This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

求C6670在ccs5上的软仿多核程序示例

你好,我刚刚开始接触C6670,希望求的一个在CCS5上的一个软仿的多核调度的程序示例!多谢!

  • mcsdk下有image process demo,这是一个带bios的多核例程,里面使用的模块比较多,可能对于初学者有点复杂。

    下面链接是一个IPC的例程用IPC reg实现核间通信,对于多核调度,对6670而言可以使用硬件队列管理器QMSS实现多核调度。

    http://www.deyisupport.com/question_answer/dsp_arm/c6000_multicore/f/53/p/1056/2535.aspx#2535

  • 你好!谢谢你,我还有些问题需要请教你!

    1. 我用的CCS5.5.0.00077_win32,在运行你给的IPC例程时,在路径File->Import->CCS->下找不到Managed Build Marcos选项,另外我的软件装在D盘的,整个D盘都没有搜索到macros.ini文件,这个文件的存在是与pdk_c6618_1_0_0_5有关的吗?pdk_c6618_1_0_0_5是个什么东西,是要另外安装还是要怎样呢?

    2. 我按照文档中的步骤软仿一个hello world,最后出现

    Can't find a source file at "/tmp/TI_MKLIBr78rCW/SRC/exit.c" Locate the file or edit the source lookup path to include its location.

    要怎么解决?

    3. 你说的mcsdk下有image process demo要怎么找到?

    不好意思,刚刚接触ccs5,和ccs3.3差别太大,很多都不明白,望详细介绍说哦!非常感谢

    C6670Helloworld工程示意图.doc
  • @

    你好,请问你的第2个问题解决了吗?

    我也出现了那个错误。

  • 把exit.c的文件路径加进去即可