你好,我刚刚开始接触C6670,希望求的一个在CCS5上的一个软仿的多核调度的程序示例!多谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!谢谢你,我还有些问题需要请教你!
1. 我用的CCS5.5.0.00077_win32,在运行你给的IPC例程时,在路径File->Import->CCS->下找不到Managed Build Marcos选项,另外我的软件装在D盘的,整个D盘都没有搜索到macros.ini文件,这个文件的存在是与pdk_c6618_1_0_0_5有关的吗?pdk_c6618_1_0_0_5是个什么东西,是要另外安装还是要怎样呢?
2. 我按照文档中的步骤软仿一个hello world,最后出现
Can't find a source file at "/tmp/TI_MKLIBr78rCW/SRC/exit.c" Locate the file or edit the source lookup path to include its location.
要怎么解决?
3. 你说的mcsdk下有image process demo要怎么找到?
不好意思,刚刚接触ccs5,和ccs3.3差别太大,很多都不明白,望详细介绍说哦!非常感谢