This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Uart boot host问题



为何我每次用“uart boot host”总提示:

(File IO): Read 198104 bytes from file F:\AllDown\Linux\uShare\aisbin_uboot0222.bin.

(Serial Port): Opening COM1 at 115200 baud...

(AIS Parse): Read magic word 0x00000021.

(AIS Parse): Boot aborted.

(Serial Port): Closing COM1.

》》我使用“\DaVinci-PSP-SDK-03.20.00.14\u-boot”编译生成bin,然后用“AISgen ”生成的bin。请问:“magic word ”是啥意思?可能是那方面的问题??