This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320C6678: SYS/BIOS使用IPC模块,将代码及数据段设置到了DDR3上的时候,核0与核1无法attach

Part Number: TMS320C6678


目前创建了两个工程,一个核0,一个核1,核0与核1之间通过ipc模块使用共享内存区域SharedRegion,调用MessageQ接口进行消息传递,若两个代码放在L2SRAM中运行,则能够正常运行;若将代码等段,通过cfg配置到DDR3中,则会出现无法attach状况,如下图所示,两个核一直无法互相attach上。

目前使用的版本信息如下:

核0代码如下:

/*
 *  ======== mutex.c ========
 *  This example shows the use of two tasks and one semaphore to perform
 *  mutual exclusive data access.
 */
#include <stdio.h>
#include <xdc/std.h>
#include <xdc/runtime/System.h>

#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>

#include <xdc/cfg/global.h>

#include "coremessage/coreipc.h"

Void task1(UArg arg0, UArg arg1);

Int resource = 0;
Task_Handle tsk1;

extern MessageQ_Handle messageQ;
/*
 *  ======== main ========
 */
int main()
{ 
    Task_Params taskParams;

    /* Create a Semaphore object to be use as a resource lock */
    InitIpc();
    /* Create two tasks that share a resource*/
    Task_Params_init(&taskParams);
    taskParams.priority = 1;
    tsk1 = Task_create (task1, &taskParams, NULL);

    BIOS_start();    /* does not return */
    return(0);
}


/*
 *  ======== task1 ========
 */
void task1(UArg arg0, UArg arg1)
{
    CoreMsg *msg;
    AttachCore(1);
    RegisterMem(0);
    MessageCreate();
    for (;;) {
        printf("Running core0 function\n");
        MessageGet(messageQ, (MessageQ_Msg*)&msg);
        printf("src:%d, flags:%d, numMsgs:%d, seqNum:%d, heartbeat:%d \n", msg->src, msg->flags, msg->numMsgs, msg->seqNum, msg->heartbeat);
        MessageFree((MessageQ_Msg)msg);
        Task_sleep(1000);
    }
}


核1代码如下:

/*
 *  ======== mutex.c ========
 *  This example shows the use of two tasks and one semaphore to perform
 *  mutual exclusive data access.
 */
#include <stdio.h>
#include <xdc/std.h>
#include <xdc/runtime/System.h>

#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>

#include <xdc/cfg/global.h>

#include "coremessage/coreipc.h"

Void task1(UArg arg0, UArg arg1);

Task_Handle tsk1;

extern MessageQ_Handle messageQ;
/*
 *  ======== main ========
 */
int main()
{ 
    Task_Params taskParams;

    /* Create a Semaphore object to be use as a resource lock */
    InitIpc();
    /* Create two tasks that share a resource*/
    Task_Params_init(&taskParams);
    taskParams.priority = 1;
    tsk1 = Task_create (task1, &taskParams, NULL);

    BIOS_start();    /* does not return */
    return(0);
}


/*
 *  ======== task1 ========
 */
void task1(UArg arg0, UArg arg1)
{
    CoreMsg *msg;
    int i = 0;
    MessageQ_QueueId QueueId;
    AttachCore(0);
    RegisterMem(0);
    MessageOpen(0, &QueueId);
    for (;;) {
        msg = MessageAlloc(0);
        printf("Running core1 function\n");
        msg->src = 1;
        msg->flags = 0x12;
        msg->heartbeat = 10 + i;
        msg->numMsgs = 1;
        msg->seqNum = i+1;
        MessagePut(QueueId, (MessageQ_Msg)msg);
        i++;
        Task_sleep(1000);
    }
}


核0,cfg文件:

mutex.cfg

核1,cfg文件:

mutex.cfg