Part Number: TMS320C6678
目前创建了两个工程,一个核0,一个核1,核0与核1之间通过ipc模块使用共享内存区域SharedRegion,调用MessageQ接口进行消息传递,若两个代码放在L2SRAM中运行,则能够正常运行;若将代码等段,通过cfg配置到DDR3中,则会出现无法attach状况,如下图所示,两个核一直无法互相attach上。

目前使用的版本信息如下:

核0代码如下:
/*
* ======== mutex.c ========
* This example shows the use of two tasks and one semaphore to perform
* mutual exclusive data access.
*/
#include <stdio.h>
#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <xdc/cfg/global.h>
#include "coremessage/coreipc.h"
Void task1(UArg arg0, UArg arg1);
Int resource = 0;
Task_Handle tsk1;
extern MessageQ_Handle messageQ;
/*
* ======== main ========
*/
int main()
{
Task_Params taskParams;
/* Create a Semaphore object to be use as a resource lock */
InitIpc();
/* Create two tasks that share a resource*/
Task_Params_init(&taskParams);
taskParams.priority = 1;
tsk1 = Task_create (task1, &taskParams, NULL);
BIOS_start(); /* does not return */
return(0);
}
/*
* ======== task1 ========
*/
void task1(UArg arg0, UArg arg1)
{
CoreMsg *msg;
AttachCore(1);
RegisterMem(0);
MessageCreate();
for (;;) {
printf("Running core0 function\n");
MessageGet(messageQ, (MessageQ_Msg*)&msg);
printf("src:%d, flags:%d, numMsgs:%d, seqNum:%d, heartbeat:%d \n", msg->src, msg->flags, msg->numMsgs, msg->seqNum, msg->heartbeat);
MessageFree((MessageQ_Msg)msg);
Task_sleep(1000);
}
}
核1代码如下:
/*
* ======== mutex.c ========
* This example shows the use of two tasks and one semaphore to perform
* mutual exclusive data access.
*/
#include <stdio.h>
#include <xdc/std.h>
#include <xdc/runtime/System.h>
#include <ti/sysbios/BIOS.h>
#include <ti/sysbios/knl/Clock.h>
#include <ti/sysbios/knl/Task.h>
#include <ti/sysbios/knl/Semaphore.h>
#include <xdc/cfg/global.h>
#include "coremessage/coreipc.h"
Void task1(UArg arg0, UArg arg1);
Task_Handle tsk1;
extern MessageQ_Handle messageQ;
/*
* ======== main ========
*/
int main()
{
Task_Params taskParams;
/* Create a Semaphore object to be use as a resource lock */
InitIpc();
/* Create two tasks that share a resource*/
Task_Params_init(&taskParams);
taskParams.priority = 1;
tsk1 = Task_create (task1, &taskParams, NULL);
BIOS_start(); /* does not return */
return(0);
}
/*
* ======== task1 ========
*/
void task1(UArg arg0, UArg arg1)
{
CoreMsg *msg;
int i = 0;
MessageQ_QueueId QueueId;
AttachCore(0);
RegisterMem(0);
MessageOpen(0, &QueueId);
for (;;) {
msg = MessageAlloc(0);
printf("Running core1 function\n");
msg->src = 1;
msg->flags = 0x12;
msg->heartbeat = 10 + i;
msg->numMsgs = 1;
msg->seqNum = i+1;
MessagePut(QueueId, (MessageQ_Msg)msg);
i++;
Task_sleep(1000);
}
}
核0,cfg文件:
核1,cfg文件: