This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AM/DM37X芯片LCD数据线格式

根据芯片手册,DISPC_CONTROL寄存器中9:8 TFTDATALINES制定DSS的数据线数目,

0x0: 12-bit output aligned on the LSB of the pixel data
interface
0x1: 16-bit output aligned on the LSB of the pixel data
interface
0x2: 18-bit output aligned on the LSB of the pixel data
interface
0x3: 24-bit output aligned on the LSB of the pixel data
interface

DISPC_GFX_ATTRIBUTES寄存器4:1 GFXFORMAT指定输出格式

0x0: BITMAP 1 (CLUT)
0x1: BITMAP 2 (CLUT)
0x2: BITMAP 4 (CLUT)
0x3: BITMAP 8 (CLUT)
0x4: RGB 12 (un-packed in 16-bit container)
0x5: ARGB16
0x6: RGB 16
0x8: RGB 24 (un-packed in 32-bit container)
0x9: RGB 24 (packed in 24-bit container)
0xC: ARGB32
0xD: RGBA32
0xE: RGBx 32 (24-bit RGB aligned on MSB of the 32-bit
container)

如果omap3evm开发版一样,并口方式,输出RGB666,配置TFTDATALINES=0x02,GFXFORMAT=0x08吗?

如果是输出RGB888,是不是就配置TFTDATALINES=0x03,GFXFORMAT=0x08就可以了呢?

是这样吗?