This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

編譯時發生can't resolve name

Other Parts Discussed in Thread: AM3359, SYSBIOS

想請問一開始編譯i2c_led範例程式時,出現一個error,叫我更新更新版的XDCTool,更新了卻出現下列錯誤

請問該如何解決?

Error

xdc.tools.configuro: InternalError: ti.platforms.evmAM3359: can't resolve name xdc.platform.IPlatform.peripherals .xdchelp /i2c_led line 51 C/C++ Problem
同樣EtherCAT Slave更新XDCtool後,沒有出現Error但沒有出現.out檔 
附件是i2c_led發生error的截圖 

====================================================

環境版本:

Win8

Hardware:AM3359 ICE v2

Software: CCS6.0

開發IDK:AM335X_StarterWare_02_00_01_01 和 am335x_sysbios_ind_sdk_1.1.0.6

BIOS:bios_6_41_02_41
XDCTOOL:xdctools_3_30_06_67_core
  • 这是使用AM335X遇到的问题吧?建议移到相应板块

  • 好的,謝謝你!

  • 请问您ccs的版本是什么? 如果也是6。0之后的,建议您clean下,再编译。

  • CCS Version: 6.0.1.00040 
    Clean過了,結果也一樣,請問不能在win8下嗎> 

  • 应该是可以的。再就是您检查下,是否有修改过代码。

    不过Win8我没有用过,公司没有win8的机器,您可以找个win7的机器试试,可以比较快的验证下。

  • 沒有修改過代碼,目前整個移除重新安裝 

  • 想請問XDC 3.23.0.26.eng要去哪裡下載,目前XDC版本都比較新了
    最新版是從這裡下載的http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/bios/sysbios/
    **** Clean-only build of configuration Debug for project ethercat ****

    "C:\\ti\\ccsv6\\utils\\bin\\gmake" -k clean
    DEL /F "ethercat.out" "configPkg\linker.cmd" "configPkg\compiler.opt"
    系統找不到指定的檔案。
    gmake: [clean] Error 1 (ignored)
    RMDIR /S/Q "configPkg\"
    系統找不到指定的檔案。
    gmake: [clean] Error 2 (ignored)
    DEL /F "tiescappl.pp" "tiescutils.pp"
    找不到 C:\ti\am335x_sysbios_ind_sdk_1.1.0.6\sdk\examples\ethercat_slave\Debug\tiescappl.pp
    DEL /F "tiescappl.obj" "tiescutils.obj"
    找不到 C:\ti\am335x_sysbios_ind_sdk_1.1.0.6\sdk\examples\ethercat_slave\Debug\tiescappl.obj
    'Finished clean'
    ' '

    **** Build Finished ****
    Buildfile generation error occurred..
    This project was created using a version of XDCtools that is not currently installed: 3.23.0.26.eng. Please install the XDCtools of this version, or migrate the project to one of the supported versions.
    Build stopped..

    以下是我目前版本

  • 用最新的版本应该是Ok的。

  • NOTE 1

    • To run on CCSv6, make sure you refactor the project after importing it
    1. Right click on imported project and select Refactor Option
    2. Select Upgrade RTSC Product Versions 

    專案>右鍵>更新就可以了
    謝謝