This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
想請問一開始編譯i2c_led範例程式時,出現一個error,叫我更新更新版的XDCTool,更新了卻出現下列錯誤
請問該如何解決?
Error
xdc.tools.configuro: InternalError: ti.platforms.evmAM3359: can't resolve name xdc.platform.IPlatform.peripherals .xdchelp /i2c_led line 51 C/C++ Problem
同樣EtherCAT Slave更新XDCtool後,沒有出現Error但沒有出現.out檔
附件是i2c_led發生error的截圖
====================================================
環境版本:
Win8
Hardware:AM3359 ICE v2
Software: CCS6.0
開發IDK:AM335X_StarterWare_02_00_01_01 和 am335x_sysbios_ind_sdk_1.1.0.6
请问您ccs的版本是什么? 如果也是6。0之后的,建议您clean下,再编译。
应该是可以的。再就是您检查下,是否有修改过代码。
不过Win8我没有用过,公司没有win8的机器,您可以找个win7的机器试试,可以比较快的验证下。
想請問XDC 3.23.0.26.eng要去哪裡下載,目前XDC版本都比較新了
最新版是從這裡下載的http://software-dl.ti.com/dsps/dsps_public_sw/sdo_sb/targetcontent/bios/sysbios/
**** Clean-only build of configuration Debug for project ethercat ****
"C:\\ti\\ccsv6\\utils\\bin\\gmake" -k clean
DEL /F "ethercat.out" "configPkg\linker.cmd" "configPkg\compiler.opt"
系統找不到指定的檔案。
gmake: [clean] Error 1 (ignored)
RMDIR /S/Q "configPkg\"
系統找不到指定的檔案。
gmake: [clean] Error 2 (ignored)
DEL /F "tiescappl.pp" "tiescutils.pp"
找不到 C:\ti\am335x_sysbios_ind_sdk_1.1.0.6\sdk\examples\ethercat_slave\Debug\tiescappl.pp
DEL /F "tiescappl.obj" "tiescutils.obj"
找不到 C:\ti\am335x_sysbios_ind_sdk_1.1.0.6\sdk\examples\ethercat_slave\Debug\tiescappl.obj
'Finished clean'
' '
**** Build Finished ****
Buildfile generation error occurred..
This project was created using a version of XDCtools that is not currently installed: 3.23.0.26.eng. Please install the XDCtools of this version, or migrate the project to one of the supported versions.
Build stopped..
以下是我目前版本