Other Parts Discussed in Thread: IWR6843
你好:
我的IWR1642功能板,在FLASH烧写的时候就有点异常,每次需要上电一点时间,才能够正常烧写,而且,程序烧写入FLASH后,不能正常上电启动,必须每次使用外部复位键复位,才能正常上电启动并工作。这是啥原因?
周正兴
20250721
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
| T3-1 | Assembled Board with an external supply current limited, turn on the DC input power; Check DC in to 3.3v | measure DCtoDC converter 3.3v out, value, ripple/noise. Record DC into 3.3v ISK board |
| T3-2 | Assembled Board, DC In applied, release PMIC NRST high, EN1 high, while keeping IWR6843 NRST low; Check DC out of PMIC 1.24v, 1.8v, 1.0v (if LDO used), 3.3v are within 2.5% of set point, use oscilloscope measure ripple, noise | measure PMIC output set point, ripple and noise; record DC current input as reset IWR current |
| T3-6 | Power up the IWR device in SOP mode 2 measure the VBAP voltage on B10 ball |
Make sure the VBGAP voltage is ~0.9V |
| T3-7 | measure the clock frequency on the CLKP pin, also CLKM if connected to crystal | The frequency should be 40Mhz |
| T3-8 | measure the WARM_RESET output, should be 6-8ms logic 1-> 0 at nRESET 0->1, Also check nERROR out = '1' | see power sequence, should be 1->0->1 |
| T3-9 | Measure the voltages on the "1p4V_APLL" and 1p4V_SYNTH" pins. | The voltages on both the pins should be ~1.4V |
| T3-10 | Using Radar Studio configure the device with the desired chirp and frame configuration; Start the chirping with infinite number of frames ; Measure the voltage on the "VOUT_PA" pin |
The voltage on this pin should be ~1V |
以上是启动前进行的测试,上电后VBGAP 是否约为0.9V
Ken
T3-1 3.3V测量值 3.312V,纹波/噪声 36mVpp;T3.2 1.2V、1.8V、1.0V、3.3V 测量值1.200V、1.798V、0.996V、3.312V;T3-6 VBGAP 电压值0.002(不启动)、0.886V(外部复位启动);T3-7 40MHz频率值 测试 无信号(不启动),测试有40MHz信号(外部复位启动);T3-8 WRAM_RESET output 0-1 at 3.3V power on(不启动) WARM_reset output 1-0-1 at 3.3V power on(启动); T3-8 1p4V_APLL 测量值0.057、1p4V_SYNTH测量值0.062(不启动)、1p4V_APLL 测量值1.421V、1p4V_SYNTH测量值1.357V(外部复位启动);T3-10 Vout_PA测量值0.023V(不启动),0.955V(外部复位启动)