Part Number: TMP235
Hi
在我用TMP235A2DBZR芯片测试PCBA温度时,供电为3.3V,一开始应用输出正常,随着温度的变化,芯片的输出很线性,温度值业很准,在某种情况下,输出会变成0.8V~1V之间,并且变化很缓慢,但是实际的温度会在此过程中迅速爬升。将芯片断电重启以后,又可以恢复正常。但是,当我尝试去复现上述现象时,很难在复现。我想知道,在什么条件或者特定情况下,芯片会出现这种情况。
谢谢!期待你的回复
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMP235
Hi
在我用TMP235A2DBZR芯片测试PCBA温度时,供电为3.3V,一开始应用输出正常,随着温度的变化,芯片的输出很线性,温度值业很准,在某种情况下,输出会变成0.8V~1V之间,并且变化很缓慢,但是实际的温度会在此过程中迅速爬升。将芯片断电重启以后,又可以恢复正常。但是,当我尝试去复现上述现象时,很难在复现。我想知道,在什么条件或者特定情况下,芯片会出现这种情况。
谢谢!期待你的回复
芯片不应具有间歇性的慢速温度响应,也不应稳定到正确的值。 在80C时,最终VOUT应约为1.3V,因此传感器稳定在0.953V时非常不正确。 您是偶尔在每个零件上看到这种情况,还是只是在某些零件上看到这种情况? 这是多么容易重现?
此外,为什么有+24V线路连接到TMP235的地面? TMP235接地是否为0伏?
那么,当24V保险丝打开/关闭时,该问题更有可能发生? TMP235需要始终连接至稳定接地才能正常工作。 如果地面移动或不是0V,则TMP235输出可能不正确和不可预测。 我知道应该没有输出锁定机制,但我认为如果您将GND连接到稳定的0V,那么这应该可以解决问题。