This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: AWR2243

Part Number: AWR2243
Other Parts Discussed in Thread: UNIFLASH

你好:

      1.在自己使用AWR2243开发的时候,是不是第一步也需要下载C:\\ti\\mmwave_dfp_02_02_02_01\\firmware\\xwr22xx_metaImage.bin的meta Image bin文件呢

      2.除了mmwavestudio还有什么办法可以下载这个bin文件呢(非级联,单片使用)

      3.这个固件内容都包含什么呢,是不是直接使用即可,无需改变,还是有什么软件可以根据不同需求设置生成这个bin文件呢

  • 问题一稍微更正下:在自己使用AWR2243开发的时候,是不是第一步也需要下载C:\ti\mmwave_studio_03_00_00_14\rf_eval_firmware\AWR2243_ES1_1\masterss和C:\ti\mmwave_studio_03_00_00_14\rf_eval_firmware\AWR2243_ES1_1\radarss的bin文件呢

  • 1. 是的。

    2. 可以通过uniflash来烧写这个bin文件到sflash。

    3. 直接使用,不需要改变。
    mmWave Firmware is responsible for configuring RF/analog, digital front end in TI mmWave radar devices and consists of below components:
     Master SS firmware (Only for AWR2243)
     Radar SS firmware (Only for AWR2243)
    All the services of Master SS and Radar SS firmware are available to external processor using the APIs in mmWaveLink framework.

x 出现错误。请重试或与管理员联系。