This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR1642BOOST: demo的输出二维数据的问题

Part Number: AWR1642BOOST


您好,

我使用的是C:\ti\mmwave_sdk_02_01_00_04\packages\ti\demo\xwr16xx\mmw

相关帖子DCA1000EVM: AWR1642EVM mmWave studio TDM or BPM MIMO setting - Sensors forum - Sensors - TI E2E support forums

我的问题在于,我在看这个用于 XWR16XX 的毫米波 (mmw) 演示中的其处理完成1DFFT之后将数据放在L3中,我认为根据上面的相关帖子来看,如果假设loopnum=32.那么TX1和TX2都将发射32个chirp,那么在放置数据的时候L3中间的箭头处将不会有空隙,如下图所示,因此该示意图是否有错误,并且这个示意图的前方的EDMApingpong操作是有问题的,不过我已经解决了前面的问题,对于后面的L3中间是否有空隙我还未得到相关答复。

下图来源于:用于 XWR16XX 的毫米波 (mmw) 演示

  • 不过我已经解决了前面的问题,对于后面的L3中间是否有空隙我还未得到相关答复

    在做完1DFFT后,配置EDMA out时使用了ping-pong机制,pong通道EDMA的dest address会按照射频参数进行调整,即

    (uint8_t *)(&rangeProcObj->radarCubebuf[samplesPerChirp * dpParams->numDopplerChirps]),所以应当无空隙