This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DCA1000EVM: 无法读取FPGA的型号

Part Number: DCA1000EVM

根据DCA1000EVM使用指南 这个网站链接进行的操作

前面的操作都已经通过

然后目前已经进行的工作:

已经改了网络连接192.168.33.30,并且关闭了防火墙

板子连接是正确的

output如下:

Fullscreen
1
2
3
4
5
6
7
8
9
10
11
12
13
14
15
16
17
18
19
20
21
GM: Constructor
GM: Sat Nov 12 22:13:47 2022
RSTD.Transmit("/Settings")
[22:13:47]
[22:13:47] ### Running Startup script: "C:\Ti\mmwave_studio_02_01_01_00\mmWaveStudio\Scripts\Startup.lua" ###
[22:13:47] RSTD.SetAndTransmit ("/Settings/Scripter/Display DateTime" , "1")
[22:13:47] RSTD.SetAndTransmit ("/Settings/Scripter/DateTime Format" , "HH:mm:ss")
[22:13:47] Scripter ignored: Attempt to UnBuild() again or before Build.
[22:13:47] RSTD.SetVar ("/Settings/Clients/Client 0/Dll" , "C:\\Ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\Clients\\\\LabClient.dll")
[22:13:47] RSTD.SetVar ("/Settings/Clients/Client 0/Use" , "TRUE")
[22:13:47] RSTD.SetVar ("/Settings/Clients/Client 1/Use" , "FALSE")
[22:13:47] RSTD.SetVar ("/Settings/Clients/Client 2/Use" , "FALSE")
[22:13:47] RSTD.SetVar ("/Settings/Clients/Client 3/Use" , "FALSE")
[22:13:47] RSTD.SetVar ("/Settings/Clients/Client 4/Use" , "FALSE")
[22:13:47] RSTD.SetVar ("/Settings/AL Client/AL Dll" , "C:\\Ti\\mmwave_studio_02_01_01_00\\mmWaveStudio\\RunTime\\SAL.dll")
[22:13:47] RSTD.SetVar ("/Settings/Clients/Client 0/GuiDll" , "")
[22:13:47] RSTD.SetVar ("/Settings/AutoUpdate/Enabled" , "TRUE")
[22:13:47] RSTD.SetVar ("/Settings/AutoUpdate/Interval" , "1")
[22:13:47] RSTD.SetVar ("/Settings/Monitors/UpdateDisplay" , "TRUE")
[22:13:47] RSTD.SetVar ("/Settings/Monitors/OneClickStart" , "TRUE")
[22:13:47] RSTD.SetVar ("/Settings/Automation/Automation Mode" , "false")
XXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXXX