您好,我在按照https://www.ti.com/lit/ug/spruij4a/spruij4a.pdf进行重新烧录的步骤的时候,在进行9.2 FPGA - SPI Flash Programming Mode的第5条的时候,点击program按钮出现如下提醒页面:

请问是哪里出现了问题呢?
首先我的连接方式如下:

点开软件的Getting Started窗口设置如下:

点开软件后整体页面显示如下:

点开软件后output显示如下:

不能识别!请问是哪里出了问题呢?
请尽快回复!
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,我在按照https://www.ti.com/lit/ug/spruij4a/spruij4a.pdf进行重新烧录的步骤的时候,在进行9.2 FPGA - SPI Flash Programming Mode的第5条的时候,点击program按钮出现如下提醒页面:

请问是哪里出现了问题呢?
首先我的连接方式如下:

点开软件的Getting Started窗口设置如下:

点开软件后整体页面显示如下:

点开软件后output显示如下:

不能识别!请问是哪里出了问题呢?
请尽快回复!
谢谢!
您好,这一步Select the bit file from the following path with the mmWave studio package: \mmwave_studio_xx_yy\mmWaveStudio\DCA1000FPGA\ DCA1000_FPGA_RECORD_xx_yy.bit file in the programming file option. (xx -> Version No, yy -> Release Date).里面的xx和yy该如何确定?这里的路径是通过选择还是可以直接输入?
第二个问题:重新烧录的FPGA会替代原先的FPGA文件?是烧录到板子上还是PC上呢?我该如何判断是否成功?
第三个问题:FPGA DONE LED (LD14)在板子哪里?我没有找到。
您好,我的结果栏从头到尾的显示如下:
Lattice VM Drivers detected (HW-DLN-3C (Parallel), HW-USBN-2B (FTDI))
INFO - Scanning USB2 Port FTUSB-0...
Programmer device database loaded
INFO - Scan completed successfully.
WARNING - Scan found ECP5UM on row 1 but cannot identify the package. Please manually select the correct device before proceeding.
ERROR - JEDEC file cannot be found.
ERROR - Check configuration setup: Unsuccessful.
INFO - Check configuration setup: Start.
INFO - JTAG Chain Verification. No Errors.
INFO - Check configuration setup: Successful.
INFO - Device1 LFE5UM-85F: Erase Only
INFO - Operation Done. No errors.
INFO - Elapsed time: 00 min : 01 sec
INFO - Operation: successful.
INFO - Check configuration setup: Start.
INFO - JTAG Chain Verification. No Errors.
INFO - Check configuration setup: Successful.
INFO - Device1 LFE5UM-85F: N25Q128A: SPI Flash Erase,Program,Verify
Initializing...
IDCode Checking...
Enabling...
Erasing...
Disabling...
Enabling...
Programming...
Disabling...
Verifying...
INFO - Execution time: 00 min : 18 sec
INFO - Operation successful with 0xF65D checksum.
INFO - Elapsed time: 00 min : 18 sec
INFO - Operation: successful.
我操作完后的FPGA DONE LED (LD14)是常亮的状态,我选择的bit文件在文件夹中上次被修改仍然是2020年(我有个疑问就是重新烧录后更新的文件是在哪里?如果不在PC端上,那么在mmwave studio里选择路径岂不是没有选上重新烧录的文件?)
我在上述步骤完成后重新试了试mmwave studio的系列操作,结果在FPGA这一步还是显示的Unable to read FPGA Version. [error -5]
结果栏显示的成功,并且我的LD14常亮,这样是烧录成功了吗?
结果栏显示成功就表示烧录成功了。
Unable to read FPGA Version. [error -5]
这个可能是其他问题了,可以看一下下面的handbook
https://dev.ti.com/tirex/explore/node?node=A__ALXBNwzujD9wALoMbM4BAQ__radar_toolbox__1AslXXD__LATEST
检查一下电脑的防火墙,杀毒软件有没有关掉?另外,看一下网线是否是直接和电脑相连的,不要使用拓展坞。
您好,请问这个文档https://e2echina.ti.com/blogs_/b/the_process/posts/dca1000evm中的第9条第四步:4)点击Browse选择相应的转储文件路径,这里的文件转储路径是指的什么路径,我这里自动显示的是:C:\ti\mmwave_studio_02_01_01_00\mmWaveStudio\PostProc\adc_data.bin,请问这个路径是否正确?如果错误我该如何选择?
您好,如您所说的话,那么我就是重新烧录正确了,但是我还是没有解决FPGA不能识别的问题,所以我将我的详细操作在这个贴子https://e2echina.ti.com/support/sensors/f/sensors-forum/466464/awr6843aopevm-fpga里的回复里进行了详细描述,希望你们能帮助我解决一下FPGA不能识别的问题,谢谢!