Part Number: AWR2944
为什么我的AWR 2944 EVM无法连接mmwave studio 3.1.1.0
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请看一下SOP[2-0]是否设置成011了?这个报错信息是在执行哪一步出错的?请看一下是否按照下面网站上的步骤操作的?
DCA1000EVM使用指南 - 嵌入式处理 - 技术文章 - E2E 设计支持 (ti.com)
(1)是将SOP设置为011,且连接无反应
执行到哪一步出错的?是否按照下面网站上的步骤操作的?
DCA1000EVM使用指南 - 嵌入式处理 - 技术文章 - E2E 设计支持 (ti.com)
(2)awr2944采集到的原始数据是只支持实数模式(only real),那请问信号的虚部是省略了吗?
那么当没有虚部的时候,如何得到信号的相位呢?
only read模式是否与复数模式相比采集到的原始数据造成了信息损失?
(3)我想通过AWR2944输出空间物体的三维坐标XYZ 请问有什么示例可以参考吗
并且不会显示设备号
是device manager里没有显示设备号吗?能否发个截图?
看一下板子的连接是否和文档里的一致?USB接的是J10口。
2.9 Connecting the AWR2944EVM to the DCA1000 EVM
https://www.ti.com/lit/ug/spruj22a/spruj22a.pdf
请看一下下面这个Note。
The EVM must be powered on before the USB cables are connected. Plugging in the USB cables before powering on the board can cause the board to get stuck in a permanent reset state. In the event that this occurs, just unplug the USB cables, power cycle the EVM, and plug in the USB cables to resolve the issue.