This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWR2243: 如果配置AWR2243让其FMCW_CLKOUT和FMCW_SYNCOUT输出20G信号

Part Number: AWR2243


您好,目前用多片AWR2243做级联,其中1片作为Master,其他作为Slave;软件上配置如下:

     1. 对Master加载了ti\mmwave_dfp_02_02_03_01\firmware\xwr22xx_metaImage.bin文件;

     2. 配置了AWR_CHAN_CONF_SET_SB的CASCADING_CFG为MULTICHIP_MASTER;

     3. 配置了CASCADING_PINOUTCFG的  bit0为0    bit1为0  bit2为0   bit3为1  bit4为1  bit5为0  bit6为1

请问这样配置是否能输出20G信号?目前我这边通过频谱仪测量不到20G信号,还可以通过哪些方法确认硬件或软件的配置是否正确?