您好,目前用多片AWR2243做级联,其中1片作为Master,其他作为Slave;软件上配置如下:
1. 对Master加载了ti\mmwave_dfp_02_02_03_01\firmware\xwr22xx_metaImage.bin文件;
2. 配置了AWR_CHAN_CONF_SET_SB的CASCADING_CFG为MULTICHIP_MASTER;
3. 配置了CASCADING_PINOUTCFG的 bit0为0 bit1为0 bit2为0 bit3为1 bit4为1 bit5为0 bit6为1
请问这样配置是否能输出20G信号?目前我这边通过频谱仪测量不到20G信号,还可以通过哪些方法确认硬件或软件的配置是否正确?