This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is Examples and Demos-"MCAN External Read Write" function normal?
SDK: MMWAVE_L_SDK_05_04_00_01
Only the transmission part of the program code is left, the details are not modified, and there is no output signal when measuring CAN TX (U5 pin.1 R78 contact)
Check s4.2->off; s1.3->on; s1.5->off.
你好,
我这里尝试过和PCAN配合,这个demo是可以正常运行的。你是否有PCAN可以测试一下?或者检查一下你的外部CAN设备。
Thanks,
Chris