This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AWRL6432BOOST: Examples and Demos-MCAN External Read Write

Part Number: AWRL6432BOOST


Is Examples and Demos-"MCAN External Read Write" function normal?

SDK: MMWAVE_L_SDK_05_04_00_01

Only the transmission part of the program code is left, the details are not modified, and there is no output signal when measuring CAN TX (U5 pin.1 R78 contact)

Check s4.2->off; s1.3->on; s1.5->off.