Is Examples and Demos-"MCAN External Read Write" function normal?
SDK: MMWAVE_L_SDK_05_04_00_01
Only the transmission part of the program code is left, the details are not modified, and there is no output signal when measuring CAN TX (U5 pin.1 R78 contact)
Check s4.2->off; s1.3->on; s1.5->off.