This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
目前我是使用AWR 2243 BOOST 以及 DCA 1000 EVM
mmwave studio 版本是3.0.0.14
DCA 1000 EVM 剛買不久
MATLAB Runtime(v8.5.1, 32-bit)
筆電為win 11
電源供應器 5V 2A
目前的output 是 Unable to read FPGA Version. [error -5]
目前已經試過
1.關防火牆
2.網路線RJ45也是直接連接在儀器上沒有使用轉接口
3.另外一臺筆電也是相同情況
想詢問如何解決 謝謝
"I am currently using the AWR 2243 BOOST and DCA 1000 EVM.
The mmWave Studio version is 3.0.0.14.
The DCA 1000 EVM was recently purchased.
MATLAB Runtime (v8.5.1, 32-bit).
The laptop runs Windows 11.
The power supply is 5V 2A.
The current output is 'Unable to read FPGA Version. [error -5]'.
I have already tried the following:
I would like to inquire about how to resolve this issue. Thank you."
你好,
电脑的杀毒软件是否有关闭后尝试?
电脑的IP地址是否配置正常?
更多信息请参考:(+) DCA1000EVM使用指南 - 嵌入式处理 - 技术文章 - E2E 设计支持 (ti.com)
Thanks,
Chris
你好,
连接有线时,请关闭无线,再尝试。
Thanks,
Chris