在对MSP430进行程序烧录时,TDC7201的GUI界面无法测时,二者是否有冲突?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好
TDC7201与MSP430结合可进行激光飞行时间测量,同时可对MSP430进行嵌入式程序烧录。具体解释如下:
TDC7201功能:TDC7201是一款高精度的时间数字转换器,特别适用于激光脉冲飞行时间测量。它作为时间测量的核心部分,能够提供极高的时间测量精度和线性度。
与MSP430结合:TDC7201通常与微控制器(如MSP430)结合使用,以构成一个完整的测量系统。在这个系统中,MSP430负责控制整个模块的工作,并处理TDC7201提供的时间测量数据。
GUI界面与程序烧录:TDC7201EVM GUI是安装在PC上的软件,用于与TDC7201模块进行通信和数据交互。同时,MSP430 LaunchPad通过USB线连接到PC上,这使得用户可以在使用GUI界面进行时间测量的同时,对MSP430进行嵌入式程序的烧录和调试。因此,TDC7201的程序并非完全封装,用户仍可通过MSP430对其进行修改和定制。
在对MSP430进行程序烧录时,TDC7201的GUI界面无法测时,二者是否有冲突?
MSP430烧录与TDC7201 GUI测时无直接冲突