This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMDSEVM6678: 关于点亮TMDSEVM6678L 评估板上的LED例程求解。

Part Number: TMDSEVM6678


新人第四天,开始练习跑灯,看了官方手册以及网上资料。

TI6678LE 评估板有7 个LED灯,那几个LED对于GPIO的引脚啊??

网上只搜到一个6678例子,例子使用的板子是创龙的DSP6678,方法如下:

开发板上的LED1和LED2是共阴极且对应GPIO14和GPIO15引脚,所以直接控制GPIO14和GPIO15输出都为高电平即可。

GPIO地址如下:02320000 023200FF 0 02320000 0 023200FF 256 GPIO。(这个我查了手册,TI6678上GPIO的地址一样),但是不知道怎么控制LED灯,求解。