This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2652R: 目前有2块CC2652R1 与2块BOOSTXL-AOA板子如何实现测量AOA角度

Part Number: CC2652R


由于AOA与CC2652R1板子连接占用了一个CC2652R1板子,官方的RLTS-AOA中好像是还需要2块CC2652板子才行(一共需要3块?)  目前我这情况可以测量出AOA角度么 还是需要再购买一块板子

  • 从SDK5.20开始,删除了AOA角度的算法,现在只提供原始IQ数据的采集

    注意要计算AOA角度,必须要有天线切换,也就是要用到天线阵列,没有天线切换就不会产生相位差,不会得到变化的角度

  • 你好,我看的是SDK5.1的版本的AOA角度计算,请问之前版本的SDK是否有我需要的例程呢?

  • SDK5.1的版本應該就有

  • 我现在是2块 CC26x2R LaunchPad    2块BOOSTXL-AOA 然后再跑 这个lab的task1-Running the AOA aplication的时候 使用了2个CC2652(其中一块外置天线接了BOOSTXL-AOA作为master 另外一块作为Slave) 然后使用可视化时候发现AOA角度 没有变化

  • * Serving Flask app "rtls_ui" (lazy loading)
    * Environment: production
    WARNING: This is a development server. Do not use it in a production deployment.
    Use a production WSGI server instead.
    * Debug mode: off
    * Running on http://127.0.0.1:5005/ (Press CTRL+C to quit)

    ----------------------- NOTE ---------------------------
    -- Chrome wasn't found in the expected path. --
    -- Open Chrome and enter URL 'http://127.0.0.1:5005' --
    --------------------------------------------------------

    127.0.0.1 - - [27/Sep/2021 10:41:30] "GET / HTTP/1.1" 200 -
    127.0.0.1 - - [27/Sep/2021 10:41:34] "GET /appVersion HTTP/1.1" 200 -
    127.0.0.1 - - [27/Sep/2021 10:41:34] "GET /rtls-ui/api/warnings HTTP/1.1" 200 -
    127.0.0.1 - - [27/Sep/2021 10:41:43] "GET /rtls-ui/api/devices-aoa HTTP/1.1" 200 -
    127.0.0.1 - - [27/Sep/2021 10:41:46] "PUT /rtls-ui/api/configuration HTTP/1.1" 200 -
    Initialization started
    Log file of current session at : E:\TI\simplelink_cc13x2_26x2_sdk_5_10_00_48\tools\ble5stack\rtls_agent\rtls_ui\logs\09_27_2021_10_41_46_log.txt
    - WebSocket Proxy Client Connected
    Initialization done
    127.0.0.1 - - [27/Sep/2021 10:41:52] "POST /rtls-ui/api/initialize HTTP/1.1" 200 -
    - WebSocket Proxy Server Started
    127.0.0.1 - - [27/Sep/2021 10:41:52] "GET /rtls-ui/api/initialize HTTP/1.1" 200 -
    Finalize started
    Receive command STOP
    错误: 没有找到进程 "raw_calculator*"。
    成功: 已终止进程 "websocket_proxy.exe",其 PID 为 29812。
    CCI Stopped
    AOA Stopped
    Finalize done
    127.0.0.1 - - [27/Sep/2021 10:41:59] "DELETE /rtls-ui/api/initialize HTTP/1.1" 200 -
    Initialization started
    Log file of current session at : E:\TI\simplelink_cc13x2_26x2_sdk_5_10_00_48\tools\ble5stack\rtls_agent\rtls_ui\logs\09_27_2021_10_41_59_log.txt
    - WebSocket Proxy Client Connected
    Initialization done
    127.0.0.1 - - [27/Sep/2021 10:42:05] "POST /rtls-ui/api/initialize HTTP/1.1" 200 -
    - WebSocket Proxy Server Started
    127.0.0.1 - - [27/Sep/2021 10:42:06] "GET /rtls-ui/api/initialize HTTP/1.1" 200 -
    Scan process started
    Scan process done
    127.0.0.1 - - [27/Sep/2021 10:42:16] "POST /rtls-ui/api/scan HTTP/1.1" 200 -
    Connection process started
    Connection Success
    127.0.0.1 - - [27/Sep/2021 10:42:18] "POST /rtls-ui/api/connection HTTP/1.1" 200 -
    Scan process started
    Scan process done
    127.0.0.1 - - [27/Sep/2021 10:43:05] "POST /rtls-ui/api/scan HTTP/1.1" 200 -
    Finalize started
    Receive command STOP
    错误: 没有找到进程 "raw_calculator*"。
    成功: 已终止进程 "websocket_proxy.exe",其 PID 为 12228。
    CCI Stopped
    AOA Stopped
    Master Disconnected
    Finalize done
    127.0.0.1 - - [27/Sep/2021 10:44:56] "DELETE /rtls-ui/api/initialize HTTP/1.1" 200 -
    Initialization started
    Log file of current session at : E:\TI\simplelink_cc13x2_26x2_sdk_5_10_00_48\tools\ble5stack\rtls_agent\rtls_ui\logs\09_27_2021_10_44_56_log.txt
    - WebSocket Proxy Client Connected
    Initialization done
    127.0.0.1 - - [27/Sep/2021 10:45:01] "POST /rtls-ui/api/initialize HTTP/1.1" 200 -
    - WebSocket Proxy Server Started
    127.0.0.1 - - [27/Sep/2021 10:45:02] "GET /rtls-ui/api/initialize HTTP/1.1" 200 -
    Finalize started
    Receive command STOP
    错误: 没有找到进程 "raw_calculator*"。
    成功: 已终止进程 "websocket_proxy.exe",其 PID 为 16312。
    CCI Stopped
    AOA Stopped
    Finalize done
    127.0.0.1 - - [27/Sep/2021 10:45:05] "DELETE /rtls-ui/api/initialize HTTP/1.1" 200 -
    Initialization started
    Log file of current session at : E:\TI\simplelink_cc13x2_26x2_sdk_5_10_00_48\tools\ble5stack\rtls_agent\rtls_ui\logs\09_27_2021_10_45_05_log.txt
    - WebSocket Proxy Client Connected
    Initialization done
    127.0.0.1 - - [27/Sep/2021 10:45:12] "POST /rtls-ui/api/initialize HTTP/1.1" 200 -
    - WebSocket Proxy Server Started
    127.0.0.1 - - [27/Sep/2021 10:45:12] "GET /rtls-ui/api/initialize HTTP/1.1" 200 -
    Scan process started
    Scan process done
    127.0.0.1 - - [27/Sep/2021 10:45:22] "POST /rtls-ui/api/scan HTTP/1.1" 200 -
    Connection process started
    Connection Success
    127.0.0.1 - - [27/Sep/2021 10:45:24] "POST /rtls-ui/api/connection HTTP/1.1" 200 -
    CCI Started
    127.0.0.1 - - [27/Sep/2021 10:45:56] "POST /rtls-ui/api/cci HTTP/1.1" 200 -
    AOA Paramas Set
    AOA Started
    127.0.0.1 - - [27/Sep/2021 10:46:01] "POST /rtls-ui/api/aoa HTTP/1.1" 200 -
    CCI Stopped
    127.0.0.1 - - [27/Sep/2021 10:48:01] "PUT /rtls-ui/api/cci HTTP/1.1" 200 -
    AOA Stopped
    127.0.0.1 - - [27/Sep/2021 10:48:04] "PUT /rtls-ui/api/aoa HTTP/1.1" 200 -
    CCI Started
    127.0.0.1 - - [27/Sep/2021 10:48:08] "POST /rtls-ui/api/cci HTTP/1.1" 200 -
    AOA Paramas Set
    AOA Started
    127.0.0.1 - - [27/Sep/2021 10:48:13] "POST /rtls-ui/api/aoa HTTP/1.1" 200 -