由于AOA与CC2652R1板子连接占用了一个CC2652R1板子,官方的RLTS-AOA中好像是还需要2块CC2652板子才行(一共需要3块?) 目前我这情况可以测量出AOA角度么 还是需要再购买一块板子
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
參考 https://dev.ti.com/tirex/explore/node?node=AOPQm8bS.juvzregJqUFPA__pTTHBmu__LATEST 的connectionless mode,RLTS-AOA只需要2块CC2652板子
我现在是2块 CC26x2R LaunchPad 2块BOOSTXL-AOA 然后再跑 这个lab的task1-Running the AOA aplication的时候 使用了2个CC2652(其中一块外置天线接了BOOSTXL-AOA作为master 另外一块作为Slave) 然后使用可视化时候发现AOA角度 没有变化
* Serving Flask app "rtls_ui" (lazy loading)
* Environment: production
WARNING: This is a development server. Do not use it in a production deployment.
Use a production WSGI server instead.
* Debug mode: off
* Running on http://127.0.0.1:5005/ (Press CTRL+C to quit)
----------------------- NOTE ---------------------------
-- Chrome wasn't found in the expected path. --
-- Open Chrome and enter URL 'http://127.0.0.1:5005' --
--------------------------------------------------------
127.0.0.1 - - [27/Sep/2021 10:41:30] "GET / HTTP/1.1" 200 -
127.0.0.1 - - [27/Sep/2021 10:41:34] "GET /appVersion HTTP/1.1" 200 -
127.0.0.1 - - [27/Sep/2021 10:41:34] "GET /rtls-ui/api/warnings HTTP/1.1" 200 -
127.0.0.1 - - [27/Sep/2021 10:41:43] "GET /rtls-ui/api/devices-aoa HTTP/1.1" 200 -
127.0.0.1 - - [27/Sep/2021 10:41:46] "PUT /rtls-ui/api/configuration HTTP/1.1" 200 -
Initialization started
Log file of current session at : E:\TI\simplelink_cc13x2_26x2_sdk_5_10_00_48\tools\ble5stack\rtls_agent\rtls_ui\logs\09_27_2021_10_41_46_log.txt
- WebSocket Proxy Client Connected
Initialization done
127.0.0.1 - - [27/Sep/2021 10:41:52] "POST /rtls-ui/api/initialize HTTP/1.1" 200 -
- WebSocket Proxy Server Started
127.0.0.1 - - [27/Sep/2021 10:41:52] "GET /rtls-ui/api/initialize HTTP/1.1" 200 -
Finalize started
Receive command STOP
错误: 没有找到进程 "raw_calculator*"。
成功: 已终止进程 "websocket_proxy.exe",其 PID 为 29812。
CCI Stopped
AOA Stopped
Finalize done
127.0.0.1 - - [27/Sep/2021 10:41:59] "DELETE /rtls-ui/api/initialize HTTP/1.1" 200 -
Initialization started
Log file of current session at : E:\TI\simplelink_cc13x2_26x2_sdk_5_10_00_48\tools\ble5stack\rtls_agent\rtls_ui\logs\09_27_2021_10_41_59_log.txt
- WebSocket Proxy Client Connected
Initialization done
127.0.0.1 - - [27/Sep/2021 10:42:05] "POST /rtls-ui/api/initialize HTTP/1.1" 200 -
- WebSocket Proxy Server Started
127.0.0.1 - - [27/Sep/2021 10:42:06] "GET /rtls-ui/api/initialize HTTP/1.1" 200 -
Scan process started
Scan process done
127.0.0.1 - - [27/Sep/2021 10:42:16] "POST /rtls-ui/api/scan HTTP/1.1" 200 -
Connection process started
Connection Success
127.0.0.1 - - [27/Sep/2021 10:42:18] "POST /rtls-ui/api/connection HTTP/1.1" 200 -
Scan process started
Scan process done
127.0.0.1 - - [27/Sep/2021 10:43:05] "POST /rtls-ui/api/scan HTTP/1.1" 200 -
Finalize started
Receive command STOP
错误: 没有找到进程 "raw_calculator*"。
成功: 已终止进程 "websocket_proxy.exe",其 PID 为 12228。
CCI Stopped
AOA Stopped
Master Disconnected
Finalize done
127.0.0.1 - - [27/Sep/2021 10:44:56] "DELETE /rtls-ui/api/initialize HTTP/1.1" 200 -
Initialization started
Log file of current session at : E:\TI\simplelink_cc13x2_26x2_sdk_5_10_00_48\tools\ble5stack\rtls_agent\rtls_ui\logs\09_27_2021_10_44_56_log.txt
- WebSocket Proxy Client Connected
Initialization done
127.0.0.1 - - [27/Sep/2021 10:45:01] "POST /rtls-ui/api/initialize HTTP/1.1" 200 -
- WebSocket Proxy Server Started
127.0.0.1 - - [27/Sep/2021 10:45:02] "GET /rtls-ui/api/initialize HTTP/1.1" 200 -
Finalize started
Receive command STOP
错误: 没有找到进程 "raw_calculator*"。
成功: 已终止进程 "websocket_proxy.exe",其 PID 为 16312。
CCI Stopped
AOA Stopped
Finalize done
127.0.0.1 - - [27/Sep/2021 10:45:05] "DELETE /rtls-ui/api/initialize HTTP/1.1" 200 -
Initialization started
Log file of current session at : E:\TI\simplelink_cc13x2_26x2_sdk_5_10_00_48\tools\ble5stack\rtls_agent\rtls_ui\logs\09_27_2021_10_45_05_log.txt
- WebSocket Proxy Client Connected
Initialization done
127.0.0.1 - - [27/Sep/2021 10:45:12] "POST /rtls-ui/api/initialize HTTP/1.1" 200 -
- WebSocket Proxy Server Started
127.0.0.1 - - [27/Sep/2021 10:45:12] "GET /rtls-ui/api/initialize HTTP/1.1" 200 -
Scan process started
Scan process done
127.0.0.1 - - [27/Sep/2021 10:45:22] "POST /rtls-ui/api/scan HTTP/1.1" 200 -
Connection process started
Connection Success
127.0.0.1 - - [27/Sep/2021 10:45:24] "POST /rtls-ui/api/connection HTTP/1.1" 200 -
CCI Started
127.0.0.1 - - [27/Sep/2021 10:45:56] "POST /rtls-ui/api/cci HTTP/1.1" 200 -
AOA Paramas Set
AOA Started
127.0.0.1 - - [27/Sep/2021 10:46:01] "POST /rtls-ui/api/aoa HTTP/1.1" 200 -
CCI Stopped
127.0.0.1 - - [27/Sep/2021 10:48:01] "PUT /rtls-ui/api/cci HTTP/1.1" 200 -
AOA Stopped
127.0.0.1 - - [27/Sep/2021 10:48:04] "PUT /rtls-ui/api/aoa HTTP/1.1" 200 -
CCI Started
127.0.0.1 - - [27/Sep/2021 10:48:08] "POST /rtls-ui/api/cci HTTP/1.1" 200 -
AOA Paramas Set
AOA Started
127.0.0.1 - - [27/Sep/2021 10:48:13] "POST /rtls-ui/api/aoa HTTP/1.1" 200 -