Other Parts Discussed in Thread: CC1350
868MHz,在HSM下,从smartRF中得到对应的功率值,配置进smartrf_settings_predefined.c中后,实际输出与表中对应值差10dB,使用芯片为4*4规格的CC1310.

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
您是在CC1310上使用HSM吗?使用配置的是SDK中的rfPacketErrorRate历程?
因为我有发现在SDK中的rfPacketErrorRate例程相关的README中有写到:HSM and OOK are not supported on the CC1310-CC1190, CC1350 (433 MHz), CC1352 (R1/P1/P-2/P-4) or CC2640R2 Launchpads。
我是否理解有误,希望您和我跟进。
您好,
我们想问您几个问题:
以下为原文: