This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC1310: 实际发射功率与配置值差10dB

Part Number: CC1310
Other Parts Discussed in Thread: CC1350

868MHz,在HSM下,从smartRF中得到对应的功率值,配置进smartrf_settings_predefined.c中后,实际输出与表中对应值差10dB,使用芯片为4*4规格的CC1310.

  • 已尝试过-10dB:0x08c0,0dB:0x0041和12dB:0xb818。均比给定值低10dB左右。

  • 您好,

    您是在CC1310上使用HSM吗?使用配置的是SDK中的rfPacketErrorRate历程?

    因为我有发现在SDK中的rfPacketErrorRate例程相关的README中有写到:HSM and OOK are not supported on the CC1310-CC1190, CC1350 (433 MHz), CC1352 (R1/P1/P-2/P-4) or CC2640R2 Launchpads。

    我是否理解有误,希望您和我跟进。

  • 是的,使用的是SDK中的rfPacketErrorRate工程,修改了GPIO适配4*4规格,我看默认发射功率给的0x23F,但我在tx table中没有找到整个对应的值,这RADEME中提到的不支持具体是指什么呢?     

  • 您好,

    RADEME中提到的不支持具体是指什么呢

    您可以在README中看到说CC1310不支持HSM,但关于这点我也要咨询一下相关产线工程师。

  • 您好,

    我们想问您几个问题:

    • 这是使用 TI 还是您定制的硬件?
    • 您是否使用 SmartRF Studio 测试了他们的电路板以对电路板进行编程(从默认设置开始)?如果没有,能否可以尝试这样做,看看测得的输出功率是多少。
    • 这些是进行的测量吗?您测量设置是什么?
    • 您能否共享这些测量结果中的任何一个(例如使用频谱分析仪的捕获)?

    以下为原文:

    • Is this using TI or custom hardware?
    • Has the customer tested their board using SmartRF Studio to program the board (starting with default settings)? If not, please can they do this and see what their measured output power is.
    • Are these conducted measurements? What is their measurement setup?
    • Can the customer share any of these measurements (a capture of their spectrum analyser, for example)?