This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

http client demo调试问题

Other Parts Discussed in Thread: CC3200

 调试设备出现这个,是因为 这个没配置好吗?,另外服务器名写IP地址的,有问题吗?
  • 请问你的HOST_NAME设置的是多少,这个就是服务器的域名,不是用IP地址。

  • 您好,我使用服务器IP能连接上

     ************************************************* CC3200 HTTP Client Application ************************************************* 
    Host Driver Version: 1.0.0.10 Build Version 2.0.7.0.31.0.0.4.1.1.5.3.3 Device is configured in default state Device started as STATION [WLAN EVENT] STA Connected to the AP: Tenda_2BD2A8 , BSSID: c8:3a:35:2b:d2:a8 [NETAPP EVENT] IP Acquired: IP=192.168.0.103 , Gateway=192.168.0.1 Connected to the AP: Tenda_2BD2A8 Connection to server created successfully
     HTTP Post Begin1: HTTP Status 200 Content-Type : application/json HTTP Post End:


    ]

    但是使用域名连接不上

    *************************************************
    CC3200 HTTP Client Application
    *************************************************

    Host Driver Version: 1.0.0.10
    Build Version 2.0.7.0.31.0.0.4.1.1.5.3.3
    Device is configured in default state
    Device started as STATION
    [WLAN EVENT] STA Connected to the AP: Tenda_2BD2A8 , BSSID: c8:3a:35:2b:d2:a8
    [NETAPP EVENT] IP Acquired: IP=192.168.0.103 , Gateway=192.168.0.1
    Connected to the AP: Tenda_2BD2A8
    Connection to server failed. error(-102)
    Error [-2011] at line [1278] in function [ConnectToHTTPServer]

  • 你使用的服务器IP多少??