This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问你的HOST_NAME设置的是多少,这个就是服务器的域名,不是用IP地址。
您好,我使用服务器IP能连接上
************************************************* CC3200 HTTP Client Application *************************************************
Host Driver Version: 1.0.0.10 Build Version 2.0.7.0.31.0.0.4.1.1.5.3.3 Device is configured in default state Device started as STATION [WLAN EVENT] STA Connected to the AP: Tenda_2BD2A8 , BSSID: c8:3a:35:2b:d2:a8 [NETAPP EVENT] IP Acquired: IP=192.168.0.103 , Gateway=192.168.0.1 Connected to the AP: Tenda_2BD2A8 Connection to server created successfully
HTTP Post Begin1: HTTP Status 200 Content-Type : application/json HTTP Post End:
]
但是使用域名连接不上
*************************************************
CC3200 HTTP Client Application
*************************************************
Host Driver Version: 1.0.0.10
Build Version 2.0.7.0.31.0.0.4.1.1.5.3.3
Device is configured in default state
Device started as STATION
[WLAN EVENT] STA Connected to the AP: Tenda_2BD2A8 , BSSID: c8:3a:35:2b:d2:a8
[NETAPP EVENT] IP Acquired: IP=192.168.0.103 , Gateway=192.168.0.1
Connected to the AP: Tenda_2BD2A8
Connection to server failed. error(-102)
Error [-2011] at line [1278] in function [ConnectToHTTPServer]