This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

协调器断电重启后,终端设备如何快速进行数据通讯?

如题,终端长poll时间为18秒。协调器断电重启后,终端设备如何保证最长18秒等待时间后进行数据通讯?

  • 跟parent node失聯後一直發beacon requests 直到重新連回網路為止
  • 如何快速找到呢?
  • 减小下面的值:


    #define REJOIN_POLL_RATE 440

    /* Rejoin retry backoff silent period timer duration in milliseconds - default 15 minutes according to HA test spec */
    #define REJOIN_BACKOFF 900000

    /* Rejoin retry backoff scan timer duration in milliseconds - default 15 minutes according to HA test spec */
    #define REJOIN_SCAN 900000

  • 在终端进入到路由设备中后,此时协调器断电重启,要等10分钟才能下发数据给终端(才有响应)【不跑到路由下面就给协调器断电可以在15秒左右就可通讯了】,请问这是什么情况,如何缩短这个时间?
  • 感覺上因為路由變了,需要時間重建路由,試試看协调器使能Many-to-One看看能不能缩短这个时间
  • uint8 zgConcentratorEnable = CONCENTRATOR_ENABLE;
    uint8 zgConcentratorDiscoveryTime = CONCENTRATOR_DISCOVERY_TIME;
    uint8 zgConcentratorRadius = CONCENTRATOR_RADIUS;
    uint8 zgConcentratorRC = CONCENTRATOR_ROUTE_CACHE; // concentrator with route cache (no memory constraints)
    uint8 zgNwkSrcRtgExpiryTime = SRC_RTG_EXPIRY_TIME;

    void ZDO_ManytoOneFailureIndicationCB()
    {
    // By default, the concentrator automatically redo many-to-one route
    // discovery to update all many-to-one routes in the network
    // If you want anything processing other than the default,
    // please replace the following code.

    RTG_MTORouteReq();----启用这个吗?
    }
  • 可以參考 www.ti.com/.../swra427c.pdf 的說明如何启用many-to-one