• TPA3118D2: 在使用TPA3118D2DAP PBTL接线方式时出现不规律咚咚咚声(敲门声)

    Part Number: TPA3118D2

    如下是我设计的原理图,请问您之前出现过类似的情况吗?

  • TPA3118D2: 是否需要和系统GND进行分地处理?

    Part Number: TPA3118D2

    您好!

    在进行音频设计这块,看到一些资料建议分地处理来防止噪声,例如codec芯片建议的布局如下,但是对于PA芯片TPA3118D2和供电不知道是否也需要进行分地处理?是否有资料可以参考?

  • TPA3118D2: 是否需要分地来隔离噪声?

    Part Number: TPA3118D2
    Other Parts Discussed in Thread: LM25118

    您好!

    对于音频Layout设计这块,CODEC是建议分地来隔离噪声,那对于TPA3118D2来说也应该要隔离到Audio GND这边,疑问是我们使用的TPA3118D2芯片的电源LM25118也要放到Audio GND这边吗?

  • TPA3118D2: 在立体声的时候,功率达到23.5W就会产生过热保护,怎样来解决

    Part Number: TPA3118D2
    Other Parts Discussed in Thread: TPA3116D2,

    在立体声的时候,功率超过23.5w,芯片就会过热保护。但规格书上面是立体声可以做到30w

  • TPA3118D2: 静音问题

    Part Number: TPA3118D2

    如图,12脚MUTE接一个100K电阻到地,不使用静音功能,这样使用是否正确。焊接好后通电没声音输出,但手碰一下MUTE脚就有输出了,再碰一下又没声音了,就像是按了MUTE按钮。手触摸一次就等于加了一次高电平。不知是什么问题,怎样才能不使用静音功能,通电就能输出音频。

  • TPA3130D2: TPA3130D2 支持PBTL吗?

    Part Number: TPA3130D2
    Other Parts Discussed in Thread: , TPA3118D2, TPA3116D2

    您好,TPA3130D2 支持PBTL吗?TPA3130D2EVM 中好像没有支持,有没有TPA3130D2 PBTL参考设计?  计划DC24V供电,负载8欧姆,失真1%情况下,可以输出多大功率?

  • TPA3118D2: The chip crashes after power-on in some uint

    Part Number: TPA3118D2

    Hi TI engineer:

          Our products have a small number of boot crashes in the process of customer use . But it didn't happen during production and testing, and more than 2,000 units of the product have been produced .

           Here are…

  • TPA3255: TPA3255Q1功放输入信号问题

    Part Number: TPA3255
    Other Parts Discussed in Thread: TPA3118D2

    我的设计是TPA3255的PBTL模式,模拟输入,但是我的输入不是差分信号,也就是INPUT_A、INPUT_B端,我只有INPUT_A有信号,INPUT_B通过一个电容接到地上,这样出来的放大信号,只有OUTPUT_A,OUTPUT_C有信号且同相,OUTPUT_B和OUTPUT_D只有一个中间电平,没有波形出来。所以想问一下,是不是哪里接错了?还是TPA3255只支持差分输入…

  • TPA3255-Q1: TPA3255的PBTL模式,模拟输入问题

    Part Number: TPA3255-Q1
    Other Parts Discussed in Thread: TPA3255, TPA3118D2

    我的设计是TPA3255的PBTL模式,模拟输入,但是我的输入不是差分信号,也就是INPUT_A、INPUT_B端,我只有INPUT_A有信号,INPUT_B通过一个电容接到地上,这样出来的放大信号,只有OUTPUT_A,OUTPUT_C有信号且同相,OUTPUT_B和OUTPUT_D只有一个中间电平,没有波形出来。所以想问一下,是不是哪里接错了…

  • TPA3118D2: 使用TPA3118D2做功放,24V供电,发热严重。

    Part Number: TPA3118D2
    Other Parts Discussed in Thread: TPA3116D2

    使用TPA3118D2做功放,双面板,24V供电,发热严重,几分钟后芯片自动重启,测试芯片表面温度到90多度。输出端接的是200W的大喇叭,现在芯片设成最小的增益(Master 20 dB R1=5.6 kΩR2=OPEN),输入正弦波幅度调到2V时,24V直流稳压源的电流为0.45A左右,TPA3118D2几分钟后直接到90多度,自动重启。如果正弦波幅度调到1V…

  • TPA3118D2: 喇叭输出脚无输出,喇叭不响,fault管脚为低电平

    Part Number: TPA3118D2

    使用tpa3118d2,喇叭输出脚无输出,喇叭不响,fault管脚为低电平

  • TPA3118D2: 供电电压由24V改为15V后,TPA3118驱动的喇叭(2X15W/4Ω)声音变小了,外围电路如下,如何改变外围电路参数让声音变大?

    Part Number: TPA3118D2

  • TPA3110D2、TPA3116D2、TPA3118D2 12V供电能有多少瓦功率输出?

    Other Parts Discussed in Thread: TPA3118D2, TPA3110D2, TPA3116D2

    TPA3110D2、TPA3116D2、TPA3118D2  12V供电4欧与8欧分别能有多少瓦功率输出?

  • 【问答互动+全新音频资料下载】便携式音频与智能语音识别

  • TPA3244与TPA3118D2

    Other Parts Discussed in Thread: TPA3244

    这两个功放芯片的功放比是多少,TPA3244内部含有一个滤波器,是不是相当于将动态滤波和功放合并在这一个芯片里面了呢?

    这两个芯片功能上最主要的区别是什么呀?哪位大神能简明的说一下,谢谢

  • 请教TPA3118/3116做单端输入的使用处理方式

    Other Parts Discussed in Thread: TPA3118D2

    请教TPA3118D2采用单端模拟输入时,只需INP端接模拟音频输入,INN端过电容接地就可以了吗?电路上需要做别的处理吗?Layout上有哪些注意的地方呢?

    多谢指教!

  • TPA3118D2 PLIMIT限制功能问题

    Other Parts Discussed in Thread: TPA3118D2

    在使用TPA3118D2 限制功率的时候,一开始给芯片供电,限制功率起到作用,但是让板子静静的待着一段时间,限制功率起不到作用,再次开机就可以了,这是什么问题,谢谢!!!

  • TPA3118D2问题求助

    Other Parts Discussed in Thread: TPA3118D2
    现使用TPA3118D2芯片,在调试过程中,发现几个问题,希望得到帮助解答。
    1、TPA3118在失真的情况下输出(LC网络以后的输出)是什么样子的波形,是对输出波形的削顶失真?还是出现一个尖峰波形?
    2、现使用的电路是TPA3118D2 EVM中的电路(http://www.ti.com.cn/cn/lit/ug/slou342a/slou342a.pdf),供电电压15V,喇叭4Ω、15W,增益比例为36dB…
  • TPA3118D2输出(带上负载)产生毛刺噪声

    Other Parts Discussed in Thread: TPA3118D2EVM

    参数:电压15V,喇叭4欧、15W,电路基本上是按照TPA3118D2EVM电路,BTL模式,后面的LC为22uh、680nF,

    产生问题现象,在某一段频率会出现毛刺波形,声音中有噪声,像是失真的样子,请问这问题出在那个方面,急需各位大神们帮助,谢谢了

  • TPA3118D2信噪比和分离度低如何解决

    Other Parts Discussed in Thread: TPA3118D2

    TPA3118D2应用电路是根据技术手册推荐电路使用的,只是把差分输入更改为单端输入,实际测试发现信噪比较低,在加权的情况下才70DB左右,分离度也达不到要求,才50DB左右,应用电路如下,请问除了布线方面的问题,还有哪些地方可以改善提高信噪比和分离度

  • TPA3118D2的SDZ和MUTE

    Other Parts Discussed in Thread: TPA3118D2

    TPA3118D2的SDZ和MUTE有什么区别吗?都是只起到静音效果吗?

  • TPA3118D2 SDZ管脚一直低电平

    如题,板子上电后无输出,发现SDZ、FAULTZ管脚一直为低电平。Sheet里列出的可能问题,一一查证后没发现问题。

    如上图所示为 我的原理图。麻烦大神看看原理图哪里有问题。谢谢~!

  • TPA3118D2 增益

    Other Parts Discussed in Thread: TPA3118D2

    请问TPA3118D2的增益只有手册上说的20dB、26dB、32dB、36dB这四种吗 不可以调试出其他的增益吗,在线等,谢谢!!

  • TPA3118D2 SYNC管脚无方波输出

    Other Parts Discussed in Thread: TPA3118D2

    大概照着芯片手册画了个板子。发现TPA3118D2 SYNC管脚无方波输出,理论上应该有100KHz方波输出。原理图如下:

  • TPA3118D2输出的LC电感选择

    Other Parts Discussed in Thread: TPA3118D2EVM

    我在使用TPA3118D2设计一个功放,要求是15V电源,4欧姆喇叭,功率在15W,BTL模式,但是在后面的LC的电感选择上出现了问题,不知道如何选择电感值的大小,还有这个电感需要是特殊的电感还是一般的电感就行?谢谢了!!我的原理图基本上按照TPA3118D2EVM设计的。

1 2 3