• LMX2820: 输出信号的dbm值,是否能在TICS-PRO中编辑,以便于我导出寄存器值去通过改寄存器值的方法来控制lmx2820输出信号的dbm值呢?

    Part Number: LMX2820

    我输入了一个10MHz的信号,通过ticspro里编辑得到寄存器值写入lmx2820模块,得到输出信号20gHz,但是输出的20gHz信号只有-40dbm,我想得调整至0dbm,请问有什么方法呢(通过调整寄存器值)?

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese…
  • LMK04610: CLKIN1输入单端100MHz正弦波,Bypass1模式下无法输出信号

    Part Number: LMK04610

    你好,

    我想用LMK04610对100MHz的时钟进行净化,该时钟为正弦波,峰峰值约3.6V,由CLKIN1单端输入,所用的VCXO也为100MHz(CVHD-950-100.000)。目前遇到的问题是我用TICS PRO将LMK04610配置为 Bypass 1(绿色),在CLKoutX测不到信号,是不是说明芯片没识别到CLKIN1端的输入信号,请问该怎么处理。

    LMK04610.zip

    TRANSLATE with x
    English
  • LMX2820: Output Doubler calibration

    Part Number: LMX2820

    HI

      I have a question about Output Doubler calibration.

      In Full Assist mode of VCO calibration type, there is no VCO calibration step, How to do Output Doubler calibration for frequency changing?

    BRs

    zhuopu

    TRANSLATE with x
  • LMK04828: 零延时规则疑惑

    Part Number: LMK04828
    Other Parts Discussed in Thread: LMK04832, LMX2594

    零延时规则要求输入时钟频率等于输出频率的最小值(GCD)。我需要进行多板同步,并且保证每次上下电时钟相位相对于参考时钟不变,所有有以下几个疑惑。

    1.想问一下这里的输入时钟频率是指的是CLK_IN还是经过R分频器后的PLL1输入频率。

    2.sync信号可以复位R分频器吗。

    3.多板同步时,需要在Setup of SYSREF Example流程中等待外部触发信号到来之后…

  • LMX2572: 请教自动斜坡参数的设置

    Part Number: LMX2572
    Other Parts Discussed in Thread: TICSPRO-SW,

    鉴相频率Fpd=100Mhz

    起始频率902.5MHz, 要求在890-915MHz之间往返扫频,步进50KHz,

    测试了几天,输出依然不对,能否帮我检查一下,或者能给予一个寄存器数值表?

    按照我的理解,

    Fstep = 0.05*4=0.2; 
    Fmax = 915*4=3660;
    Fmin = 890*4=3560;
    Fstart = 3610;

    RAMP_LIMIT_HIGH…

  • LMH1983: PLL1输出时钟调整

    Part Number: LMH1983

    我输入信号为1080P29.97的HVF信号,输出时钟硬件连接的是PLL1的out,怎么配置可以让PLL1输出的时钟变成27M/1.001,而不是27M。

    我猜测是应该需要把AFD功能取消,强制配置PLL1的R N,比如设置为900,那此时输出的就是29.97*900=26.973M

    请问该如何实现这个需求

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi
  • LMK05318BEVM: 1PPS phase detector的值和参考晶振之间的关系?

    Part Number: LMK05318BEVM

    1PPS phase detector的值和参考晶振之间的关系是怎么样的,比如我使用的是12mhz的tcxo晶振那我应该选择多大稳定度的晶振才能够实现锁定,这个值又是如何计算的。我之前使用12mhz的晶振可以成功锁定。我当时保存了相应配置文件,但一个月后我重新导入配置文件。1pps信号却始终无法成功锁定,所以我想知道这个问题的原因,麻烦您解答一下,并给出能够成功锁定的方式,我是否需要更换晶振。以下是我所用晶振的datasheet,辛苦您了,万分感谢…

  • CDCE72010: CDCE72010的主参考时钟振幅限制

    Part Number: CDCE72010

    CDCE72010的差分输入PRI_REF,振幅被限制在0.1~1.3V之间,外部晶振产生的时钟源很难有如此小的幅值差,请问该如何解决?

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw Romanian
    Chinese Simplified Hungarian Russian
    Chinese…
  • LMK04803: Phase noise data of internal VCO

    Part Number: LMK04803

    Dear Team,

    I want to design a phase-locked loop circuit. In order to determine the appropriate loop bandwidth so that the phase noise of the output signal is low, I need to know the phase noise data of the internal VCO of the LMK04803…

  • LMK04828: LMX2594如何配置输出时钟

    Part Number: LMK04828
    Other Parts Discussed in Thread: LMX2594

    Hi,

       下面框图是想要实现的输出时钟,TICS pro能导出文件直接烧录到芯片中还是在线写寄存器?谢谢!

  • LMX2694-EP: muxout输出状态异常

    Part Number: LMX2694-EP

    在2694锁定正常的状态下,断开外部100MHz参考,有很大几率muxout输出还是2.8V,而非正常的0V,请问如何避免?寄存器配置如下:

    R114 0x720000
    R113 0x710000
    R112 0x700000
    R111 0x6F0000
    R110 0x6E0000
    R109 0x6D0000
    R108 0x6C00F1
    R107 0x6B0000
    R106 0x6A0007
    R105 0x694440
    R104 0x680000
    R103 0x6700…

  • LMX2594: 信号测量与波形配置

    Part Number: LMX2594
    Other Parts Discussed in Thread: LMX2492, , LMX2572

    您好,请帮忙回复以下问题:

    1.LMX2594EVM中章节“F 斜升功能”中,图“F-2”的时频图是用什么软件或仪器测试的?

    2.配置类似斜升波形时,能否设置仅上升ramp输出相应频率的信号,而在下降ramp不输出信号?

  • LMX2820: 输出波形和EVM不一样

    Part Number: LMX2820
    Other Parts Discussed in Thread: TPS62152

    我在LMX2820EVM上使用默认配置时,输出6G信号很理想,但在我自己的板子上使用TICS pro的默认配置输出波形有很大的抖动,下面附图片,请问这是为什么?

  • LMX2572: 请问我现在项目中有需要使用2颗LMX2572 在一个小的PCB内,请问布局需要怎么处理才能减少相互的串扰

    Part Number: LMX2572

    目前用2颗LMX2572 在同一个小的PCB内,请问布局需要怎么处理才能减少相互的串扰,特别是电源和GND的布线,PCB叠层是否有推荐,谢谢 ,

    补充一下项目中要求频率输出6.4G和6.398GHz

  • LMK3H0102: TICS PRO中的PCIE Refence Clock analysis tool,生成PCIE时钟report失败?

    Part Number: LMK3H0102

    把PNA测试的LMK3H0102产生的100M时钟的测试数据(.csv) 导入到TICS PRO中的PCIE Refence Clock analysis tool中,但是生成报告失败,请问如何解决?

    CSV文件格式如下:

    Center Frequency [Hz]
    99752047.11
    Frequency [Hz] Phase Noise [dBc/Hz] Phase Noise - no spurs [dBc/Hz…
  • LMX2592: 与lmx2592锁定与锁定完与马上不锁定的情况

    Part Number: LMX2592

    lmx2592芯片编程进行锁定,锁定时会有小灯亮起,一直锁定一直亮,我进行编程后小灯刚开始会亮起,但不到几秒就会暗淡下去,而我进行示波器进行观察后发现,正确的图时有一高点并且一直不动,而我的图是有这个高点但是这个高点与整个上升图会向右进行平移

    TRANSLATE with x
    English
    Arabic Hebrew Polish
    Bulgarian Hindi Portuguese
    Catalan Hmong Daw
  • LMK1D1208: Inquiry Regarding LMK1D1208 Buffer Output Issues

    Part Number: LMK1D1208

    Dear TI Technical Support Team,

    I am currently working on the schematic design for the LMK1D1208 buffer. I have selected a 3.3V single-ended LVCOMS signal as the input, based on the device specifications. However, I have encountered…

  • LMX2820: 如何降低±5~20MHz的spur

    Part Number: LMX2820

    如附圖,我在專案中需要使用LMX2820提供LO訊號

    但以10MHz為一點掃過9~18GHZ

    發現部分頻率會出現主tone±5~20MHz 大小約-60~-80dBc不等的spur,

    例如附圖1中為19.41GHz在±5MHz 有大小約-68dBc的spur

    嘗試不同配置如附圖2在±5MHz 也有大小約-73dBc的spur

    想請問這類的spur產生是我配置上有誤

    還是我有什麼方法能將spur抑制在-85dBc以下嗎…

  • LMX2594: 配置寄存器后,始终锁不住,但是在输出端用示波器能测量到信号

    Part Number: LMX2594

    配置寄存器后r110[10:9]始终为11,请帮忙看看配置哪里有问题,三种vco assist方式都试过,输入oscin为100M,产生一路5000M时钟和一路12.5M sysref

    寄存器配置如下:

    R112 0x700000
    R111 0x6F0000
    R110 0x6E0400
    R109 0x6D0000
    R108 0x6C0000
    R107 0x6B0000
    ///read back register


    R106 0x6A0000
    R105 0x69002…

  • LMX2694-EP: 输出4.3G信号中有很多杂散

    Part Number: LMX2694-EP
    Other Parts Discussed in Thread: PLLATINUMSIM-SW

    大家好:

    在使用LMX2694-EP芯片输出信号时,测试500-6000M频段输出是,发现部分频段信号近端有杂散,比如在4300MHz时,杂散离主信号最近;

    查了些资料,好像是PLL的整数边界杂散(IBS, Integer Boundary Spurs),即鉴相频率及其谐波和输出信号杂散,如112.88*35-4300=0.8M;

    减小电荷泵电流可以减小点杂散…

  • lmk04828数字延迟功能使用不了

    Other Parts Discussed in Thread: LMK04828, LMK04832

    各位专家。我这边正在验证lmk04828的数字延迟和模拟延迟。输入为clkin1输入20mhz时钟,oscin输入为100mhz时钟。vco0为2500mhz。

    dclkout0为2500mhz,dclkout2为2500mhz。我使用示波器测试这两个时钟的延迟。

    关于模拟延迟。我在TICSPRO上设置clock output  select设置为analog delay + divider。在芯片配置完成后…

  • LMX2820EVM: 即时校准与相位同步原理

    Part Number: LMX2820EVM
    Other Parts Discussed in Thread: LMX2820

    HI Team

    1. 请问LMX2820即时校准的原理是什么?

          我现在可以使用即时校准的方式进行跳频,但是我不理解即时校准锁定的原理

    2. 请问LMX2820相位同步的原理是什么?我想更加深入了解一下

    谢谢

  • LMK05318B: synchronization questions

    Part Number: LMK05318B

    Hi,

    I have some questions about the synchronization capabilities of LMK05318B devices.

    When I use the 1pps clock of GPS as a reference input, there are several questions that I don't understand all the time

    1. OUT7 of 05318B…

  • LMX2820: 计算步进与实际测得值不一样

    Part Number: LMX2820

    PFD= 10Mhz, 固定三阶调制器,FDEN=2^32-2,此时 步进=10*10^6/(2^32-2)=0.0023hz,但这个时候,使用单片2820,测出生成的频率值频率偏移不是这个值

  • LMX2820EVM: 即时校准时间问题

    Part Number: LMX2820EVM

    即时校准的锁定时间问题

    我使用TICS Pro模拟即时校准,并用示波器抓取TP_LD的低电平脉冲宽度

     

    TICS Pro采用以下推荐的配置流程,流程来自于链接回复:LMX2820: LMX2820 not locking with instant calibration - Clock & timing forum - Clock & timing - TI E2E support forums

     

    After a Vcc power…

1 2 3 4