输出频率5.9~7.5G,采用single pfd模式,RFoutA直接输出,RFoutB输出经16分频后得到368.75~468.75M,给AD9912提供参考,再由AD9912产生50M信号,与一个固定500M信号混频到550M信号,送至PFDIN,经内部11分频至50M与OSCIN输入的50M信号鉴相,VCO采用强制模式,如5.9~6.35选择VCO1,6.35~7.3选择VCO2,配置后,仅5900M附近几十M能锁定,其他都不锁定。配置寄存器如下…
输出频率5.9~7.5G,采用single pfd模式,RFoutA直接输出,RFoutB输出经16分频后得到368.75~468.75M,给AD9912提供参考,再由AD9912产生50M信号,与一个固定500M信号混频到550M信号,送至PFDIN,经内部11分频至50M与OSCIN输入的50M信号鉴相,VCO采用强制模式,如5.9~6.35选择VCO1,6.35~7.3选择VCO2,配置后,仅5900M附近几十M能锁定,其他都不锁定。配置寄存器如下…
我设置为双缓冲模式 用tics_pro控制的时候可以实现锁频,然后对小数寄存器写值,在写R0寄存器,发现频率发生了改变。但是当我将这些操作搬到fpga的时候,在没扫描的时候是能锁频的,一旦快速更新小数寄存器和R0寄存器的值以后,就会无法锁定频率,没有输出。 怎么搞?
我输入了一个10MHz的信号,通过ticspro里编辑得到寄存器值写入lmx2820模块,得到输出信号20gHz,但是输出的20gHz信号只有-40dbm,我想得调整至0dbm,请问有什么方法呢(通过调整寄存器值)?
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese… |
HI
I have a question about Output Doubler calibration.
In Full Assist mode of VCO calibration type, there is no VCO calibration step, How to do Output Doubler calibration for frequency changing?
BRs
zhuopu
大家好!
问题:LMX2820的VCO倍频输出频率11.3GHz~22.6GHz范围内存在失锁现象,回读R74寄存器,rb_LD的值为3,即为Invalid,读到的LD引脚(PIN38)也为低。且失锁后必须复位才能重新控制其它频率至锁定状态。复位导致锁定时间频率切换的锁定时间太长,难以接受,希望得到TI官方的回复,此芯片是否存在这个缺陷,是否有办法解决,还是说控制上面有问题?
测试方法:11.3GHZ~22.6GHz范围内以1MHz的步进进行自动测试,失锁时中断自动测试…
我需要将-2~2dBm的50欧姆的100MHz信号,给4个锁相环(例如LMX2820)作为输出参考。请教下,是否需要增加buffer,或者放大器,有推荐型号么。或者是否放大器+功分器也可以呢?
您好,在使用LMX2820时,电荷泵的输出会出现如图所示的情况,无法检测到锁定,输出的频率也与我目标的有些差距,请问是什么问题呢,感谢您的回答。 另外我的环路滤波器与EVM板上一致,参考时钟信号为差分,Vpp=400mV。
Hi,
We find that when setting frequencies of 4160MHz,at -10℃,LMX2820 can not be locked.
Could you tell me how to resolve this?Thanks so much.
如附圖,我在專案中需要使用LMX2820提供LO訊號
但以10MHz為一點掃過9~18GHZ
發現部分頻率會出現主tone±5~20MHz 大小約-60~-80dBc不等的spur,
例如附圖1中為19.41GHz在±5MHz 有大小約-68dBc的spur
嘗試不同配置如附圖2在±5MHz 也有大小約-73dBc的spur
想請問這類的spur產生是我配置上有誤
還是我有什麼方法能將spur抑制在-85dBc以下嗎…
We set up a board with lmx2820, the software can not control the output at present. But register reads and writes are normal. For example, reset=1 and R0=0x4070.
We did a few things on R32, 36, 42, 43, 38, 39, 78, 79,0, but RFOUTX_P…
根据手册上所说,LMX2820作为单端输出时,未使用的一端:将此引脚端接到看起来与所使用输出相似的负载。这通常是一个交流耦合到地的 50Ω 电阻器。这是为了尽量减少谐波。
在使用时,如果没有将未使用端的做等长布线而是就近做了交流耦合50Ω到地,这会对2820的单端输出造成功率上的或者其他影响吗
I need to use the instant calibration function of lmx2820. After initialization according to the following steps, I turned the POWERDOWN up to reduce power consumption, and then changed the frequency, but the frequency could not be…
HI Team
1. 请问LMX2820即时校准的原理是什么?
我现在可以使用即时校准的方式进行跳频,但是我不理解即时校准锁定的原理
2. 请问LMX2820相位同步的原理是什么?我想更加深入了解一下
谢谢
PFD= 10Mhz, 固定三阶调制器,FDEN=2^32-2,此时 步进=10*10^6/(2^32-2)=0.0023hz,但这个时候,使用单片2820,测出生成的频率值频率偏移不是这个值
即时校准的锁定时间问题
我使用TICS Pro模拟即时校准,并用示波器抓取TP_LD的低电平脉冲宽度
TICS Pro采用以下推荐的配置流程,流程来自于链接回复:LMX2820: LMX2820 not locking with instant calibration - Clock & timing forum - Clock & timing - TI E2E support forums
After a Vcc power…
Hi Team:
1. 我在这个文档里面看到LMX2820的原始的无辅助校准时间为 153 μs
但是我在TICS Pro中模拟了此过程,测试条件如下,校准时间达到了200us,我又试了45M--55M的跳频时间,校准时间超过了350us
测试方法:只更改图中位置,其他位置不做修改,并且开启了所有的影子寄存器,用示波器抓取TP_LD引脚的低脉冲宽度
请问为什么我的测试结果与文档中描述不符…
您好,我参考开发板手册搭建了测试环境,实际相噪结果与手册所给结果相差16dB左右,请问是什么原因。
测试环境如下:
电源:KEYSIGHT E36313A 3.3V/0.6A
基准源:LEYSIGHT PSG 100M
仿真软件:TiCS Pro
信号分析仪: CEYEAR 4141F
测试频点:6GHz
测试相噪点:10KHz频偏处
问题:实际测试结果为-100dBc/hz@10khz,理论结果为-116dBc/hz@10khz,为何相差甚大…
你好: 我现在使用LMX2820,用正常模式,想要什么频点 ,是可以锁住的,但是用PFDIN 外部反馈模式 ,确怎么也锁定不了,我没有使用即时校准功能 这个可以
这个不行
使用TICS Pro控制锁定后出现一定范围(300Hz以上)频率漂移,为什么会发生这种现象?
Hi Team:
1,输入Fosc=100M,分母设置=1000*1000,最小分辨率为100Hz;
2,测试中发现,如果设置200M+100Hz,LMX2820正常输出,状态锁定;
3,若设置为200M-100Hz,LMX2820无法输出,LDpin状态不锁定;但是Reg74中的rb_LD为0x2,指示为锁定;
4,分析了一下,发现当设置200M-100Hz时,分子的数值比较大,为NUM=999968,INSTCAL_PLL_NUM=4294829824…