This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1672驱动问题

Other Parts Discussed in Thread: ADS1672

最近在使用TI的ADS1672。用CPLD(MAXII)驱动。ADC的工作时钟是20M,采用外部读时钟也是20M。

现在的问题是读的数据有时候会出错。每次读1024个数据就会有三四个不正常数据(此数据很大或者很小)。

我把驱动文件贴出来放附件里。还有就是Read引脚我用的是低脉冲触发的那个引脚。望大神教我。

第一次在TI论坛发帖,教教我


module ads1672_drive( sys_clk20m,   //CPLD系统时钟
                      sys_rst,      //CPLD复位信号
							 ready_port,   //数据采集完成端口
							 data_port,    //数据采集端口
							 
							 device_cs,    //器件片选
                      work_clk20m,  //ADS1672工作时钟
							 read_clk20m,  //数据读时钟
							 Buffer_24bit  //实时采集的数据
                     );
							
input  sys_clk20m;
input  sys_rst;
input  ready_port;
input  data_port;

output reg device_cs;	
output work_clk20m;
output read_clk20m;	
output reg [23:0] Buffer_24bit;


      reg  Pulse_NowSta;  //ready的脉冲最新状态
      reg  Pulse_OldSta;  //ready的脉冲前一状态
      wire Rising_Edge;   //上升沿
      wire Falling_Edge;  //下降沿

      assign work_clk20m = sys_clk20m;
	
      always@( posedge sys_clk20m or negedge sys_rst)
            if( !sys_rst) begin
               Pulse_NowSta<=1'b1; //这两个状态的初始值和信号源的初始状态总是一致的,才是最安全的
               Pulse_OldSta<=1'b1;
            end
            else begin
               Pulse_NowSta<=ready_port;
               Pulse_OldSta<=Pulse_NowSta;
            end
       
      assign Rising_Edge =(~Pulse_OldSta)&Pulse_NowSta; 
      assign Falling_Edge=(~Pulse_NowSta)&Pulse_OldSta; 
		
		//读取24bit数据需要24个时钟,数据读完毕需要关闭读时钟
		reg        ReadClk20m_EN;   
		reg  [4:0] ReadClk20m_Cnt;
		
		reg Buff_Sta;
		
		always@( posedge sys_clk20m or negedge sys_rst)
            if( !sys_rst ) begin 
				     device_cs    <=1'b1;    
				     ReadClk20m_EN<=1'b0; 
				end
            else begin
				     if( ReadClk20m_Cnt==5'd24 ) begin 
					      device_cs    <=1'b1; 
					      ReadClk20m_EN<=1'b0;
				     end 
				     else if(Falling_Edge )  device_cs<=1'b0;
				     else;
			        if(Rising_Edge)         ReadClk20m_EN<=1'b1;
				end 
/*
		always@( posedge sys_clk20m or negedge sys_rst)
            if( !sys_rst )	                Buff_Sta<=1'b0;
				else if(ReadClk20m_Cnt==5'd24) Buff_Sta<=1'b0;
				else if(ReadClk20m_EN)         Buff_Sta<=1'b1;
				else                           Buff_Sta<=1'b0;
*/				
		 assign read_clk20m=(ReadClk20m_EN==1'b1)?sys_clk20m:1'b0; 
				 
		
       reg [23:0] Temp_Buff; //24bit数据读取临时缓存 
	  
		 //数据采集	
	    always@( posedge sys_clk20m or negedge sys_rst)
             if( !sys_rst )	begin
				     ReadClk20m_Cnt<=5'd0;
					  Temp_Buff     <=24'd0;
					  Buffer_24bit  <=24'd0;
			    end 	
				 
				 else begin
				      if(ReadClk20m_EN) begin
						
						   ReadClk20m_Cnt<=ReadClk20m_Cnt+1'b1;
							
							case(ReadClk20m_Cnt) 
						  
						      0: Temp_Buff[23]<=data_port;
							   1: Temp_Buff[22]<=data_port;
							   2: Temp_Buff[21]<=data_port;
							   3: Temp_Buff[20]<=data_port;
								
							   4: Temp_Buff[19]<=data_port;
							   5: Temp_Buff[18]<=data_port;
							   6: Temp_Buff[17]<=data_port;
							   7: Temp_Buff[16]<=data_port;
								
							   8: Temp_Buff[15]<=data_port;
							   9: Temp_Buff[14]<=data_port;
							  10: Temp_Buff[13]<=data_port;
							  11: Temp_Buff[12]<=data_port;
							  
							  12: Temp_Buff[11]<=data_port;
							  13: Temp_Buff[10]<=data_port;
							  14: Temp_Buff[9] <=data_port;
							  15: Temp_Buff[8] <=data_port;
							  
							  16: Temp_Buff[7] <=data_port;
							  17: Temp_Buff[6] <=data_port;
							  18: Temp_Buff[5] <=data_port;
							  19: Temp_Buff[4] <=data_port;
							  
							  20: Temp_Buff[3] <=data_port;
							  21: Temp_Buff[2] <=data_port;
							  22: Temp_Buff[1] <=data_port;
							  23: Temp_Buff[0] <=data_port;
							  
							  24: begin 
							           Buffer_24bit<=Temp_Buff;
										 // Buffer_24bit<=24'd98765;
										  ReadClk20m_Cnt<=5'd0;
								   end 
									
							 default: ;
						  endcase
						end 
				 end 

endmodule