This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1298: ADS1298导联脱落检测不到的问题

Part Number: ADS1298


使用ADS1298芯片,芯片使用正负2.5V供电,发现三个问题。

第一个问题:RA导联脱落检测不到,电流源导联脱落和上拉下拉电阻脱落都试了,读到的LOFF_STATN寄存器的数值都是0,但是设置导联脱落翻转寄存器让电阻翻转时,能读到RA准确的脱落状态,原理图、寄存器配置如下:

当设置电阻翻转之后,读到的状态字如下:

第二个问题:RL导联脱落读到的状态字和ALL脱落的状态字一样,如下图所示:

第三个问题:每隔24秒钟,输出端的数据就会有一次比较大的跳动,持续大概几百毫秒,但是把输入端短路之后,就不会再出现,把数据转换为波形之后如下所示:

希望得到解答,多谢!