TI专家,您好!我们有两个问题想咨询一下:
1、ADS1299规格书显示最大放大倍数只有24,那么如果想采集到uV级别的微弱EEG信号,这是否意味着需要在ADS1299外部,即脑电极之后另外加前置放大电路?或者说ADS1299芯片内部在PGA之前有其他放大电路?因为在芯片框图中没有看到相关前置放大单元,麻烦解惑一下!
2、ADS1299EEGFE-PDK user's guide第7页3.1.1节介绍 “Microsoft® Windows® XP…
TI专家,您好!我们有两个问题想咨询一下:
1、ADS1299规格书显示最大放大倍数只有24,那么如果想采集到uV级别的微弱EEG信号,这是否意味着需要在ADS1299外部,即脑电极之后另外加前置放大电路?或者说ADS1299芯片内部在PGA之前有其他放大电路?因为在芯片框图中没有看到相关前置放大单元,麻烦解惑一下!
2、ADS1299EEGFE-PDK user's guide第7页3.1.1节介绍 “Microsoft® Windows® XP…
寄存器读出来全是零,使用软件显示这个错误是什么情况啊
Arabic | Hebrew | Polish |
Bulgarian | Hindi | Portuguese |
Catalan | Hmong Daw | Romanian |
Chinese Simplified | Hungarian | Russian |
Chinese Traditional | Indonesian | Slovak |
Hello,
I want to use STM32F411 to drive ADS1299 for 8 channel data acquisition.
How should I do it? Where can I get some guidance?
Looking forward to your reply.
HuY
DYDR引脚应接入菊花链的主设备中,上述原理图中,已发现DYDR引脚接错,接到了从设备中
是不是因为该引脚接错而导致读取寄存器的值错乱呢
除了上述问题,对基于该原理图,能否给我一些改进的建议呢
我现在使用ADS1299设计了8通道脑电采集电路板。在测试电路性能的时候,我使用信号发生器输出10Hz、2mV的标准正弦波形,信号发生器的正极依次连接1-8通道,信号发生器的负极与电路参考SRB2相连,以测试每个通道的性能。结果通道1到通道7都输出了标准正弦波形,但是通道8中噪声干扰较大、波形畸变。
为了避免通道串扰、电磁干扰,我把通道8前端的电阻电容全都挖掉了,通道8前端没有任何元件连接。信号发生器的输出直接接到芯片ADS1299的通道8引脚,结果还是一样噪声干扰很大…
Hello!
ADS1299IPAGR We found that the wafer mold void after X-RAY, this is normal? Can you provide information to explain?
Hello,
I would like to know if ADS1299 can perform neural extracellular recording?
Is it possible to realize this application using ADS1299EEGFE-PDK?
Hello,
I would like to know if ADS1299 can perform neural extracellular recording?
Is it possible to realize this application using ADS1299EEGFE-PDK?
在学校打算用ADS1299作为传感器核心电路来做一个自制的EEG脑电波检测帽
但是我在翻芯片的时候看到TI专门给AFE4960解决EEG提供了一个解决方案的帖子,链接如下:可穿戴脑电图 (EEG) (Rev. B)
想问一下,对于未来想入职脑电帽相关行业的研究生来说,选择哪款芯片比较好(对比图如下)。以前相关的项目经历局限于EOG和一些嵌入式开发,请教路过的工程师,…
已经成功读取到了内部测试信号的矩形波,但幅值范围有问题,我设置增益为24,测得的信号单边幅值为0.000018V,正常应该为0.0018V,设置寄存器chnset = 0x61,增益为24,测量内部噪声,八个通道的噪声范围在-0.00089V~-0.00009V,之后又测量了MVDD模式,发现无论设置增益为1还是24,八个通道的输出都是直接达到上限(增益为1时是4.5V,增益为24时是0.1875V),想问下这是什么原因,有什么解决方法。
void startADS(void)
{
Transfer_START();
HAL_Delay(10);
Transfer_RDATAC( );
HAL_Delay(10);
HAL_Delay(100);
}
void Transfer_START(void)
{
SPI1_CS_0();
SPI1_ReadWriteByte(_START);
HAL_Delay(100);
SPI1_CS_1();
}
void Transfer_RDATAC(void…
设计过程中考虑两个问题:
TI工程师
您好!
我有以下3个问题请教:
1、我这边按照下图参考连接N端,芯片N端脚外部还需要连接AVDD吗?
2、用菊花链方式连接2颗芯片,两颗芯片的SRB1需要连接到一起吗?通道连接两颗芯片都参照问题1图。
3、如果共用第一颗芯片的bias偏置驱动,是否第二颗芯片的biasout、biasin两个角就不需要接了,仅连接两颗芯片biasinv即可?
…
TI工程师
您好!
我有以下3个问题请教:
1、我这边按照下图参考连接N端,芯片N端脚外部还需要连接AVDD吗?
2、用菊花链方式连接2颗芯片,两颗芯片的SRB1需要连接到一起吗?通道连接两颗芯片都参照问题1图。
3、如果共用第一颗芯片的bias偏置驱动,是否第二颗芯片的biasout、biasin两个角就不需要接了,仅连接两颗芯片biasinv即可?
…
您好
我们在使用ADS1299芯片进行阻抗测量,使用一个500k电阻进行测试,使用N作为输入端时可以正常测量出阻抗,电路连接如下
其中P端未使用,通过芯片内部SRB2连接作为参考电极;
但当我们改变接线方式,使用P端作为输入时,测量500k电阻得到的阻抗值约为21000,与实际值相差过大,电路连接如下
其中N端未使用,通过芯片内部SRB1连接作为参考电极;
我们验证过正常测量信号时均正常,只有在测量阻抗时存在较大的差异,请帮忙分析一下
TI工程师
您好!
我这边使用1299搭建16通道脑电采集系统,发现通道采集的波形是斜的,原始AD值就是斜的,未做任何处理。请问是什么原因呢?以下是波形图,采样电机、参考电极、驱动电极均空置(没有带在头上)
使用自製的PCB版,檢測輸入點電壓都沒問題,如圖1到圖3
圖1.(DVDD,3.3V)
圖2.(AVDD,2.5V)
圖3.(AVSS,-2.5V)
圖4.VCAP1
圖5.VCAP2
圖6.VCAP3
圖7.VCAP4
圖8.Vref
根據[FAQ] ADS1298: ADS129x:如何验证 ADS129x 器件是否仍然正常工作? ,檢測內部電壓節點,發現VCAPx 都有問題
ADS1299的 連接 VCAP1 的電容C22跨壓卻是0V,C22兩端皆為-2.5V,連接 VCAP2…
使用ADS199FE-PDK 透過SPI連接到 STM32F4052的開發版,mcu spi baud rate設置為2M,CPOL=LOW,CPHA=2 Edge,我開啟八通道的test signal輸入,使用邏輯分析儀發現每個通道的值差異不大,如圖1,但在每個SPI傳輸後,使用UART讓藍芽傳輸,SPI的值就會變得很奇怪,如圖二,請問是正常的嗎?
以及我該如何檢驗SPI的結果是正確的呢,謝謝